STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

scope question on variable wrt I2C ??

I have the following two wrapper functions:void POT_Load_Value(uint16_t value) { uint8_t w[2]; w[0] = 0; //reg w[1] = value; I2C_Write(POT_ADDR, w, 2); }   uint8_t I2C_Write(uint8_t device, uint8_t *pValues, uint8_t size) { if (HAL_OK == HAL_I2C...

SWenn.1 by Senior III
  • 939 Views
  • 1 replies
  • 0 kudos

In STM32G474 ,CORDIC module for trigonometric functions

In STM32G474 , I used CORDIC module for trigonometric functions calculations but this module requires fixed point represntation and i store the final value in float variable . can the transformations between fixed point to float point be done using a...

AIBRA.1 by Associate II
  • 1400 Views
  • 1 replies
  • 1 kudos

STM32F051K6 I want to set to 32bit TIMER for TIM2

Hi ,I am trying to set STM32F051K6  to 32bit TIMER for TIM2. what register needs to be set in-order to count to 32bit mode. I read the HRM but there is not detailed description where to set TIM 2 to 32bit mode.

ck.1 by Associate III
  • 1555 Views
  • 2 replies
  • 0 kudos

.data �?역�?� 2개�?� Memory �?역�? 할당하는 방법

안녕하십니까?STM32H743�?� 예로 들 경우,​MEMORY{RAM_D1 (xrw) : ORIGIN = 0x24000000, LENGTH = 512KRAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288KRAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K}​​와 같�?� �?역�?� 있�?� 때, RAM_D1�?� 공간�?� 부족하여​.data 섹션�? 대해서 RAM_D1과...

How to use dfu in project to flash the uC

I need to do an upgrade of the firmware via software. From my C++ app i have to call dfu-util, i guess, or if there is any other way please let me know, to download the upgrade to the uCFor the moment i am calling it like a system call, and i wonder ...

EPop.2 by Associate II
  • 2046 Views
  • 4 replies
  • 0 kudos