STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to read ADC values

Hi Im Lalin, Im using STM32L433RC-P MCU for learning.Im facing the issue in reading the data from ADC.Im not getting any error too.Below are the source code attached.Kindly help me to find the solution for this.Note that im using uart.c for debugging...

STM32H742 TIMER CLK 50MHz frequency

I am using the STM32H742 MCU.Currently, System CLOCK is set to 480 MHz and APB TIMER and AHB maximum CLK is set to 240 MHz.However, the maximum frequency of TIMER and GPIO cannot exceed 25 MHz, so what should I do to make it over 50 MHzAttached is th...

eogos_0-1758702607455.png eogos_1-1758702626863.png
eogos by Associate II
  • 1038 Views
  • 7 replies
  • 0 kudos

Resolved! i2c dma question

Hi i'm using STM32F411RE. I've been reading data from ADC IC using I2C communication. It's 400Khz, and I'm reading using DMA. By the way, if another interrupt with high priority occurs during I2C communication, it runs that interrupt during I2C commu...

giwonKIM by Associate III
  • 928 Views
  • 5 replies
  • 5 kudos

Resolved! CAN wrong bit timing: bit time larger than expected

Title edited to give an accurate idea of the issue. Hello together, i had a problem with setting a correct bit time on a CAN-port. On my nucleo-h755ZI-Q board, I want to operate the FDCAN1 by the CM4 in classic-can mode with a baud rate of 1 MHz. I s...

HiSt_0-1759130563982.png HiSt_1-1759130584276.png HiSt_2-1759130618964.png HiSt_3-1759130645218.png
HiSt by Associate III
  • 1198 Views
  • 9 replies
  • 1 kudos

HRTIM Start Synchronization

Hi All. So, I'm currently working on a project that I need some assistance with... I'm using the HRTimer and ADC. Timer A and Timer E both control my gate drive outputs; they're variable frequency. I also have Timer F, which controls my ADC sampling....

Jbin0101 by Associate III
  • 2331 Views
  • 2 replies
  • 0 kudos

Resolved! Bad voltage on VREF+ pin (VDD instead of VREFBUF)

I'm using an STM32H743VIT6 (rev V in LQFP100 package), powered at 3.3V and programmed with STM32CubeIDE.I'm using the ADC2 and ADC3, and also want to use the VREFBUF voltage (available on VREF+ pin) programmed for 2.5V. The *.ioc file is generated wi...

FRAUBRY by Associate II
  • 6700 Views
  • 17 replies
  • 4 kudos