STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bad voltage on VREF+ pin (VDD instead of VREFBUF)

I'm using an STM32H743VIT6 (rev V in LQFP100 package), powered at 3.3V and programmed with STM32CubeIDE.I'm using the ADC2 and ADC3, and also want to use the VREFBUF voltage (available on VREF+ pin) programmed for 2.5V. The *.ioc file is generated wi...

FRAUBRY by Associate II
  • 6700 Views
  • 17 replies
  • 4 kudos

Resolved! Has ChatGPT bricked my NUCLEO-L433RC-P board :(

I wanted to do a full chip erase using STM32Programmer (I am trying to debug a custom bootloader) but kept getting the error "Mass erase operation failed.  Please verify flash protection".I sent the following option byte screenshot to ChatGPT....Chat...

freeflyer_3-1758476281788.png

STM32F446RET6 Timer and clock

Hi,  I designed the us and ms delay functions using timer 2 and 4. Initially in the PLL source, I was using HSI, but it had some errors, so I switched it to HSE. I was using my delay function to control the DAC output, but when I switched to HSE, all...

Junzhe_0-1758900040115.png Junzhe_1-1758900047568.jpg Junzhe_2-1758900122851.png Junzhe_4-1758900460320.png
Junzhe by Associate II
  • 470 Views
  • 1 replies
  • 0 kudos

Resolved! NOR Flash on OSPI bus with ST MX25UM51245G Library

Hello, I am struggling to use the following ST library for a project I am working on, I am using an stm32u5 with an MX25UM51245G NOR chip connected to the OSPI1 bus.  The library provided is setup to use XSPI_HandleTypeDef, Can this library be used w...

brohr01 by Associate III
  • 614 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F4 marking

标准时间(标准时间)的标签产地和芯片产地不一样,请问这个是否正常 Translation: The label on this device (Standard Time Clock) indicates different countries of origin for the product and the chip. Is this normal? Edited by ST moderator. In next time please use English as this is an i...

xuzejian by Associate II
  • 3243 Views
  • 5 replies
  • 2 kudos