STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563 bootloader command over SPI

Based on the information found in AN4286 rev 14, I am trying to command to bootloader to start executing the application.The setup is a H573 and a H563 connected over SPI @ 0.5 MHz. The 573 operates as SPI master, and the 563 as a slave. I know that ...

Dimlite by Associate III
  • 3328 Views
  • 2 replies
  • 2 kudos

Resolved! STM32f4 ADC DMA Discontinuities

I have a problem and currently no clue how to further debug. Maybe one coudl help me. I use STM32f4 to capture with ADC1 3 signals with 1Mhz (so 333kHz per channel) triggered by a timer and transfered via DMA. I have a DMA buffer of 3*2*100 (so 100 s...

BastelBaus_0-1759491791658.png BastelBaus_1-1759491864289.png BastelBaus_2-1759491888224.png BastelBaus_3-1759491900824.png

Resolved! STM32H7 programming w/out STLINK

Hiya. This is my first time working with custom STM PCBs.I was planning on flashing/programming my custom STM32H7 board (specifically STM32H7A3RGT6) over STLINK and then just do general purpose programming over the USB-C COM Port. However, the TAG co...

Resolved! How to flash STM32F429zi nucleo via UART without ST-Link?

Hello,I'm working with STM32F429ZI nucleo board, and I would like to flash my program using UART (USART1 or UART3 via  a usb to ttl converter)  instead of ST-Link.I understand that STM32 has a built-in bootloader that can be used for flashing via UAR...

Asha1 by Associate
  • 1109 Views
  • 3 replies
  • 3 kudos

Resolved! Dual core concurrent access to the same FMC memory address

Hello, We have a STM32H755 with an FRam (similar to SRAM) module attached to the FMC. We have been seeing CPU exceptions when the M4 core tries to access (read only) the same memory location the M7 core is writing to. So, it seems that the FMC does n...

scuba by Associate II
  • 1414 Views
  • 8 replies
  • 1 kudos

I²C on STM32C011 using PC14 (SDA) not working

Hello,I am working on an STM32C011 (Nucleo-like custom board) and trying to use I2C1 with the following pinout:PB7 → I2C1_SCL (AF14)PC14 → I2C1_SDA (AF14)According to the reference manual / datasheet, PC14 can be mapped as I2C1_SDA (AF14).I connected...