User Activity

Hi Team,We are using the STM32H753VIH6 in our design.We are having MAC to MAC connection with Realtek GMAC port and STM MAC port.The schematics connections is in the attachment.Now we would like to generate 50MHz reference clock from STM32 to Realtek...
Hi Team, we are using the STM32H753VI in our design.we are not using the USB interfaces.In this case, what is the termination to be done to the VDD33USB pin of STM whether it can be NC, GND? ThanksManikandan R
 Hi Team, We are using the VL53L4CX in QCS8550 platform.Below are queries listed below for clarification. Query 1:Load Capacitance I'm using a same I2C for 5 sensors of VL53L4CX. Is that good to connect or any load capacitance issues will occur Need ...