STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DFU Download & Upload only 1024-byte page works

Hello, I'm using WinUSB and I'd like to program the flash memory at address 0x0800c0000 in 256-byte increments. This works fine the frame but every frame after this gets written to blocks in increments of 1024. It seems that if one needs to push more...

Resolved! STM32H503 simultaneous ADC and DAC use

I've spent some time recently trying to prototype a small project based on the STM32H503 which would need to have the ADC and DAC running simultaneously with multiple channels of analog I/O via DMA. I was able to get this all coded up but discovered ...

Resolved! RTC_OUT availability while STM32H7 is powered off

Hi,I'm using an STM32H7 microcontroller and need to get the RTC working.I set RTC_OUT to 1Hz and set the LSE to a 32.768Hz crystal, and inserted the CR2032 battery.When the microcontroller is powered (VDD 3V3), I see the waveform oscillating at a fre...

AndreaTW by Associate II
  • 4380 Views
  • 3 replies
  • 0 kudos

GPIO change Mode without losing the charge

Hello everybody,I'm trying to get from a pulled up state / driven up state to a tristate pin without losing the charge that is on that pin.It seems to me, that whenever a pullup is deactivated (PUPDR), that STM32 will first discharge the pin and then...

THein.3 by Associate II
  • 734 Views
  • 6 replies
  • 1 kudos

MCU Selection High Speed SPI and QSPI

Hello Team,We are Looking to select MCU Which has High Speed SPI and QSPI in a Single Device ,High Speed SPI - 50 Mbps to 90 Mbps ( One channel ) to interface External Ethernet Controller QSPI  - ( One channel ) -  to interface with External Motion U...

bsuthar by Senior
  • 594 Views
  • 2 replies
  • 0 kudos

Resolved! STM32C011 "Can not read memory"

I designed simple board around STM32C011J6 MCU (SO8 package). I'm using fresh-from-packaging parts, ordered from Element14 (Farnell). When I try to connect to MCU (via SWD, using ST-LINK/V2 ISOL), I get "Can not read memory! Disable Read Out Protecti...

torasn by Associate
  • 603 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H7 MCU selction: HRTIM with DLL?

Title and content edited: modified MPU by MCU. There is a big differenece between MPU and MCU products Hi,   we are currently selecting an STM32 MCU.   We need a dual core M7+M4 and so we've spotted STM32H757, so far so good. Unfortunately we (lately...

Tototo_0-1759398552874.png
Tototo by Associate
  • 1169 Views
  • 2 replies
  • 1 kudos