STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! RXP bit not being after SPI transfer

Hello all, I have been struggling with DMA transfers from SPI transactions and would love a second opinion on what I could be doing wrong. I have confirmed that polling works and I can corroborate the data I see in the RX registers with a scope. I do...

JCori by Associate II
  • 1110 Views
  • 8 replies
  • 0 kudos

Both OCTOSPI ports memory mapped on STM32H7A3?

Hello,I am having trouble memory mapping both OSPI ports at the same time. Can I run a QSPI Flash on OSPI1 and a OSPI Hyperbus RAM on OSPI2 and have both be memory mapped or do both OSPI ports need to be running in the same mode to be memory mapped?T...

DWWelch by Associate III
  • 943 Views
  • 5 replies
  • 3 kudos

Resolved! STM32C092 (TSSOP20) FDCAN Bootloader

Hi everyone, i just want to be sure cause it's the first time playing with the bootloader.I have a STM32C092 (TSSOP20) an i was wondering if i can flash it through FDCAN, but reading the AN2606 i unfortunately found a postilla as following (page71):F...

Sanderthunder_0-1759876921686.png

Resolved! L1 EEPROM: same as L0 ?

Heyho,still checking L1 for new project, next question:Are the L1's internal EEPROM register interface, erase, read, and write functions the same as on L0 (we're already using that) ?Obrigado!

LCE by Principal II
  • 594 Views
  • 7 replies
  • 4 kudos

Resolved! DMA Freezes CPU STM32F401

I am using STM32F401, I had an application which communicates via USART1 by using DMA2. Both RX and TX DMAs are working fine. So I added a bootloader and moved application to 0x08008100. Bootloader is using same USART1 and DMA2. Now bootloader is wor...

alig_ones by Associate II
  • 1001 Views
  • 7 replies
  • 3 kudos

Resolved! Question on Flash-to-Flash IAP on STM32F303CC

Hello everyone,I'm working on an In-Application Programming (IAP) solution for an STM32F303CC. I've divided the flash memory into two application areas (let's call them App1 and App2), and I want to rewrite the program in App2 from code running in Ap...

Thatcher by Associate II
  • 864 Views
  • 5 replies
  • 1 kudos