STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with understanding UART interface

I have a device made of two modules. Each module has its own ST microcontroller, family is STM32L476. They are connected together with a cable of 2-2.5 meter coated, most likely, with a silicone tube.I need to make the two microcontrollers communicat...

mdiro by Associate III
  • 5850 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F730xx ADC: EOC never set when reading VREFINT

Hello,we want to read VREFINT to make our ADC measurements more accurate.But the EOC bit is never set when selecting the ADC_CHANNEL_VREFINT channel.PCLK2 is at 108MHz but ADC prescaler and sampling cycles are at max. so we assume there is no problem...

rengl by Associate II
  • 3263 Views
  • 6 replies
  • 0 kudos

Resolved! Bug Report: STM32 H723ZG wrong register name, FTHVL <-> FTHLV

In some places the register name "FTHLV" is typed wrong:The right register name is "FTHLV": In STM32 CubeIDE the name is wrongly spelled "FTHVL": In the Reference Manual RM0468 (Page 2227) it is one time called "FTHLVL": And in another Diagram (Page ...

_legacyfs_online_stmicro_images_0693W00000bimMBQAY.png _legacyfs_online_stmicro_images_0693W00000bimMkQAI.png _legacyfs_online_stmicro_images_0693W00000bimMzQAI.png _legacyfs_online_stmicro_images_0693W00000bimNJQAY.png
DBeck.7 by Associate
  • 3511 Views
  • 2 replies
  • 0 kudos

Resolved! Issue with the RTC REF_IN on STM32F439NIHx

Hi,I'm having some trouble with trying to correct the RTC drift on a STM32F439NIHx. I've enabled the REF_IN and provided a 50Hz signal on the pin, but the RTC still drifts by around 1s per day.I've also tested that the 50Hz signal is correctly receiv...

DPitt.2 by Associate II
  • 5545 Views
  • 17 replies
  • 0 kudos

The DMA transfer only the first byte from ADC1 (STM32H735)

I configure the ADC1 of the STM32H735 like bellow:The ADC Clock = 20MHzADC_HandleTypeDef hadc1; DMA_HandleTypeDef hdma_adc1;   /* ADC1 init function */ void MX_ADC1_Init(void) {   /* USER CODE BEGIN ADC1_Init 0 */   /* USER CODE END ADC1_Init 0 *...

_legacyfs_online_stmicro_images_0693W00000biUC8QAM.png _legacyfs_online_stmicro_images_0693W00000biUKvQAM.png
Saif by Associate II
  • 6718 Views
  • 19 replies
  • 0 kudos