STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! board(B-L475E-IoT01A), I use the AWS package demo to connect to the AWS IoT, after I configured all in the tera term, it show the error "WARN: setRTCTimeDateFromNetwork L#84 Could not find hostname ipaddr www.gandi.net". How to solve it ?

I first use the default RootCA1, device certificate and private key to configure, but it show the error:"WARN: setRTCTimeDateFromNetwork L#84 Could not find hostname ipaddr www.gan";Then I follow the readme, and use the"Amazon1_Usertrust_Baltimore.cr...

_legacyfs_online_stmicro_images_0693W00000bkU6nQAE.png _legacyfs_online_stmicro_images_0693W00000bkU6sQAE.png
lzhij.2 by Associate II
  • 1829 Views
  • 1 replies
  • 0 kudos

Unable to debug STM32 BlackPill

Hi!So i am new to this STM32 family. I purchased a blackpill with STM32F401CCU6. I am trying to get the printf working on it. I followed multiple resources to get it working which included the ITM Data Trace, OpenOCD semihosting, UART, etc. Some chan...

klug by Associate
  • 2897 Views
  • 2 replies
  • 0 kudos

getting same unique ID for different controllers

Hi everyone, can anyone pls help me with the problem, i'm trying to read the unique ID of the stm32U585 controller, i'm able to read the ID with HAL functions, but im getting the same output for all the three different controller with different syste...

meghasb by Senior
  • 2228 Views
  • 4 replies
  • 0 kudos

H745 Timer DMA Output Capture Artifact

I have a project where I need to output a precise waveform to drive some external FETs and thought this would be a good opportunity to fill a DMA buffer with CCR values and tie this to TIM2 that is configured with output capture on channel 1. Just fo...

SPetr.6 by Associate III
  • 1566 Views
  • 1 replies
  • 0 kudos

LPTIM interrupt can't wake STM32u5 from STOP low power mode

I am trying to us the LPTIM low power timer to trigger interrupts intermittently while the MCU is in STOP2 mode, but I am unable to do so. I am testing the interrupts by toggling a GPIO pin and checking the output on a scope.Without STOP mode I see t...

_legacyfs_online_stmicro_images_0693W00000bkEVhQAM.png
JKahn.1 by Associate III
  • 5776 Views
  • 5 replies
  • 1 kudos

Higher Baud Rate using SmartCard with Clock in ISO7816-3

Hi @ChannelI am trying to interface SAM Module TDA8026 with STM32U585 and have few doubtsAny support in this regard(Reference, example library etc)As per the ISO 7816 standard - maximum frequency of clk should be less than 5MHz with default fi and di...

PJose.4 by Senior
  • 2156 Views
  • 1 replies
  • 0 kudos