Skip to main content
AElta.1
Associate II
Sep 11, 2022 3:35 PM UTC
Question

Read parallel data that is valid in every falling edge clock nucleo-h743ZI2

Hello

I have an external adc with 2 parallel output pins each is 1 bit (2 bits) total, with clK_out pin, I am trying to read the parallel pins using nucleo-h743ZI2 (480Mhz), I followed [AN4666] example to receive the data1, clk_out is connected to PA6 which is defined as a TIMER in input capture and it triggers the DMA to GPIO pins and save it into memory. Unfortunately my code read the pins only once and I was expecting that it would read every falling edge of the clk_out. all I trying to do is make the dma read every falling edge. here is my code I would really appreciate all the help I can get.

#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
 
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define MAX_FRAME_SIZE 100
#define BUFFER_SIZE 20
#define HALF_BUFFER_SIZE BUFFER_SIZE/2
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
volatile int LastITHalfComplete = 0;
volatile int32_t FullDataIndex = 0;
volatile int i = 0;
volatile uint8_t transferComplete = 0;
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_ch1;
 
UART_HandleTypeDef huart3;
 
PCD_HandleTypeDef hpcd_USB_OTG_FS;
 
/* USER CODE BEGIN PV */
static uint8_t aFull_Buffer[MAX_FRAME_SIZE] = {0};
static uint8_t aDST_Buffer[BUFFER_SIZE] = {0};
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART3_UART_Init(void);
static void MX_USB_OTG_FS_PCD_Init(void);
static void MX_TIM1_Init(void);
static void MX_DMA_Init(void);
/* USER CODE BEGIN PFP */
static void TransferComplete(DMA_HandleTypeDef *hdma_tim1_ch1);
static void TransferError(DMA_HandleTypeDef *hdma_tim1_ch1);
static void HalfTransferComplete(DMA_HandleTypeDef *hdma_tim1_ch1);
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_USART3_UART_Init();
 MX_USB_OTG_FS_PCD_Init();
 MX_TIM1_Init();
 MX_DMA_Init();
 /* USER CODE BEGIN 2 */
 // Attach DMA callback functions
 	htim1.hdma[TIM_DMA_ID_CC1]->XferHalfCpltCallback = HalfTransferComplete;
 	htim1.hdma[TIM_DMA_ID_CC1]->XferCpltCallback = TransferComplete;
 	htim1.hdma[TIM_DMA_ID_CC1]->XferErrorCallback = TransferError;
 
 	// Start DMA in interrupt mode, specify source and destination
 
 	HAL_DMA_Start_IT(htim1.hdma[TIM_DMA_ID_CC1], (uint32_t) &GPIOC->IDR, (uint32_t) &aDST_Buffer, 1);
 
 
 	// Enable timer to trigger DMA transfer - CC1DE bit
 	__HAL_TIM_ENABLE_DMA(&htim1, TIM_DMA_CC1);
 
 	// Enable timer input capture
 	HAL_TIM_IC_Start(&htim1, TIM_CHANNEL_1);
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 	 /* USER CODE BEGIN WHILE */
 		while (1) {
 			//if (transferComplete) {
 				//transferComplete = 0;
 				// Transmit buffer to UART
 				// Prepare data into buffer
 				//HAL_UART_Transmit_IT(&huart3, buff, LEN);
 			//}
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 		}
 /* USER CODE END 3 */
}

the interrupts

static void HalfTransferComplete(DMA_HandleTypeDef *hdma_tim1_ch1) {
	int position = 0;
	 LastITHalfComplete = 1;
	 /*Copy the first part of the received buffer */
	 for (int i = 0; i < HALF_BUFFER_SIZE; i++)
	 {
	 aFull_Buffer[FullDataIndex] = aDST_Buffer[i+position];
	 FullDataIndex++;
	 HAL_GPIO_TogglePin(GPIOE, GPIO_PIN_1);
}
 
}
static void TransferComplete(DMA_HandleTypeDef *hdma_tim1_ch1) {
	int position = HALF_BUFFER_SIZE;
	 LastITHalfComplete = 0;
 
	 /* Copy the second part of the received buffer */
	 for (int i = 0; i < HALF_BUFFER_SIZE; i++)
	 {
	 aFull_Buffer[FullDataIndex] = aDST_Buffer[i+position];
	 FullDataIndex++;
	 HAL_GPIO_TogglePin(GPIOB, GPIO_PIN_0);
	 }
 
 
	transferComplete = 1;
}
 
static void TransferError(DMA_HandleTypeDef *hdma_tim1_ch1) {
	HAL_GPIO_TogglePin(GPIOB,GPIO_PIN_14);
}
 
void HAL_UART_TxCpltCallback(UART_HandleTypeDef *huart3) {
	// Enable again DMA for a new transfer
	HAL_DMA_Start_IT(htim1.hdma[TIM_DMA_ID_CC1], (uint32_t) &GPIOC->IDR, (uint32_t) aDST_Buffer, BUFFER_SIZE);
}

Thank you in advance

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
Dec 23, 2022 1:28 PM UTC

Hello @AElta.1​,

Which STM32CubeMX version are you using?

If you use the STM32CubeMX 6.7.0 ​ version could you please share the .ioc file?

Try to move the MX_DMA_Init(); line code before MX_USART3_UART_Init(); in your main.c.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.