STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7B0 (A0). Is it possible to copy data from an sdcard to an external qspi rom to be used as program rom (.romdata)?

Is it possible to copy data from an sdcard to an external qspi rom to be used as program rom (.romdata)? I am currently reading data from an sdcard card using fatfs to const program in the. (.data) section but it is a memory hog. Are there any examp...

I have an issue with the HAL_DMA_TransmitReceive() function. I am using full-duplex SPI communication between STM32F030R8T6 as master, and Nucleo-C031C6 as slave. I am only using DMA on the master side. My DMA clock is at 40MHz, SPI clock is at 10MHz.

The problem is I can successfully transmit-receive up to 4 bytes of data. Above that amount, anomalies happen. I need to transfer 20 bytes of data in both directions. Does this have anything to do with RXFIFO and TXFIFO buffers being 4 bytes, or is i...

DDjur.1 by Associate II
  • 1966 Views
  • 4 replies
  • 0 kudos

Can't get ADC values

I have an STM32G474RE, I have not used any HAL or LL libraries, I have only programmed using the registers, my issue is that I am only getting 0 on the output of the ADC, I read through the reference manual and still couldn't solve the problem. I hav...

_legacyfs_online_stmicro_images_0693W00000dDeuQQAS.png
Epsilon03 by Associate II
  • 5828 Views
  • 8 replies
  • 0 kudos

DMA is jamming the RTC

Hello, I have a problem with RTC and UART reception using the DMA.I am currently working with the L476RG core board. The RTC clock is the LSE. The UART is configured in cyclic mode on the Rx PIN.I have done a simple data logging and could check that ...

_legacyfs_online_stmicro_images_0693W00000dDcblQAC.png _legacyfs_online_stmicro_images_0693W00000dDccKQAS.png
JFlui.1 by Associate II
  • 1568 Views
  • 2 replies
  • 0 kudos

Resolved! How to call timer interrupt using registers? [NO HAL DRIVERS]

Hi, i am trying to call timer interrupt handler using registers and the following is my code, but the problem is that the function is being not called, I see no output in the oscilloscope or live expression. First my DAC value is still 0, the counter...

RShre.2 by Associate III
  • 5403 Views
  • 7 replies
  • 0 kudos

Resolved! How to read GPIO direction using HAL?

Hello world,I'm developing a FW for STM32F107VCT6 which can change GPIO direction programmatically: there is a terminal command which can switch individually 7 pins* mapped on different ports between GPIO_MODE_OUTPUT_PP \ GPIO_MODE_INPUT.I'm wonderin...

Spaghetto by Associate III
  • 3052 Views
  • 3 replies
  • 2 kudos