STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Programing firmware

I am developing a board using the STM32H725. We are currently programing each board using the STM32Cube    programmer and then we send the PCB on a test bench to test each card. This step that seems to be quite simple but it actually adds additional ...

josimmor by Associate
  • 4056 Views
  • 2 replies
  • 1 kudos

ADC noise on STM32F413

Hello,For a project (control motor application), we are using ADC from MCU STM32F413. We encounter some noise on ADC measurments. We observe to high standard deviation on our ADC result.We show in errata doc of mcu  we an issue: "Internal noise impac...

AlexisC by Associate II
  • 4736 Views
  • 9 replies
  • 0 kudos

UPGRADE FIRMWARE stm32l072kztx

Olá pessoal, estou tentando atualizar o micro firmware usando stm32 cubeIde stm32l072kztx. Já tentei usar os comandos AT^SISS e baixar o arquivo .HEX compilado via FTP, já tentei usar os comandos AT^SNFOTA, mas não funcionou. Baixando via FTP consigo...

STM32 MCUs

Hi,I want to use input capture mode using TIMER2 feature of Stm32f730vbt6 microcontroller. I am receiving a pulse signal from the oscilloscope and I want to remove it via STM using the timer's input capture mode. What should I use in the code for thi...

Leylifer by Associate II
  • 2016 Views
  • 2 replies
  • 0 kudos

AMS5812 I2C Sensor Holding I2C3 Bus on STM32F407G-DISC1

I am trying to implement LCD and AMS5812 Sensor on I2C3 Bus,But AMS5812 I2C sensor is holding the I2C bus and preventing further scanning STM32F407G Discovery board.  /*-[ I2C Bus Scanning ]-*/ HAL_UART_Transmit(&huart2, (uint8_t *)StartMSG, s...

asking_0-1694252450817.png asking_1-1694252475072.png
asking by Associate III
  • 10099 Views
  • 9 replies
  • 0 kudos

Resolved! STM32F756 Alternate function

Hi there, i come across AN4760 p55, configuring GPIOB with alternate functions :GPIOB->AFR[0] = 0x0A000900;  where does this 0A000900 come to config PB2 n PB6 to QSPI alternate function?GPIOB->AFR[1] = 0x00000000; ....GPIOF->AFR[0] |= 0x9900000000;  ...

StanJerm by Associate III
  • 6587 Views
  • 4 replies
  • 0 kudos

Resolved! Timer compare function interrupt not triggered sometimes

Hi everyone, I meet a problem and I'm not sure it's MCU issue or I program not proper.I meet this issue both on the STM8 and STM32 MCUs.I enable TIM_2 Ch1 as input to capture the signal and TIM_2 Ch2 as output to do the compare function. void init_TI...

Joey_Duh by Associate II
  • 8152 Views
  • 11 replies
  • 3 kudos