2023-05-11 1:28 AM
I want to update ARR new value when timer eneble(counter is counting). What can I do to update it quickly without time latency (like setting the UG bit) ? I am using stm32f0.
2023-05-11 3:33 AM
Don't set TIMx_CR1.ARPE.
Be warned, that if you set ARR to value below CNT, in that cycle CNT will count up to the maximum for given timer (i.e. 0xffff for 16-bit timer or 0xffffffff for 32-bit timer) (purpose of ARR preload is exactly to prevent this).
JW