Skip to main content
MOhamed_Mehery
Associate III
May 11, 2023
Solved

What is the use of STM32L452 VDD12 pin, why should I put 1.2 voltage regulator to supply this pin?

  • May 11, 2023
  • 1 reply
  • 911 views

..

This topic has been closed for replies.
Best answer by Sarra.S

Hello @MOhamed_Mehery​,

First, VDD12 is only available on packages with the external SMPS supply option. 

Also, it is not necessary to wire this pin, you can use it, if you want to improve the power consumption, especially in Run and Sleep mode.

In that case, there are 3 SMPS ranges to supply VDD12, please check RM0394 section 5.1.6

Hope that helps!

1 reply

Sarra.SBest answer
ST Employee
May 11, 2023

Hello @MOhamed_Mehery​,

First, VDD12 is only available on packages with the external SMPS supply option. 

Also, it is not necessary to wire this pin, you can use it, if you want to improve the power consumption, especially in Run and Sleep mode.

In that case, there are 3 SMPS ranges to supply VDD12, please check RM0394 section 5.1.6

Hope that helps!

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.