STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H563 UART DMA idle not triggering

Hello everyone,I'm working on a custom board with an STM32H563 and using CubeMX, HAL, and ThreadX.I am trying to receive variable-length UART data via DMA using HAL_UARTEx_ReceiveToIdle_DMA(). My problem is that the HAL_UARTEx_RxEventCallback never t...

kasjdlfkjsadfjl.png WhatsApp Image 2025-11-08 at 06.23.47.jpeg
mipi by Associate
  • 973 Views
  • 2 replies
  • 1 kudos

Resolved! Duplicated Virtual COM Port number on Windows

I have several an 2 F401RE boards connected to my PCs and getting data by the Virtual Communication Port.Unfortunately when installing a new board on the PC, I ve seen that my 2 boards were declared by Windows with the COM portCOM port 7, 9 and 10 ar...

PoP_0-1762982372832.png
PoP by Associate II
  • 903 Views
  • 3 replies
  • 4 kudos

Single shot timer for peripheral timeout check

Hello,I'm here on H75x. I'm looking for portable way to do a timeout check via timer.Here, I want a timeout IRQ if UART receive DMA hangs up.First I setup a OnePulse timer in Cube. It generates the following code:if (HAL_TIM_Base_Init(&htim6) != HAL_...

regjoe_0-1752772838108.png
regjoe by Senior II
  • 2169 Views
  • 17 replies
  • 2 kudos

Resolved! 1.8V VDD and 3.3V VUSB

Hi,I’m using an STM32L052 with LQFP32 package, VDD = 1,8V.According to the datasheet:“VDD_USB = 1.65 to 3.6V: external power supply for USB transceiver, USB_DM (PA11) and USB_DP (PA12). To guarantee a correct voltage level for USB communication VDD_U...

amel by Associate
  • 720 Views
  • 3 replies
  • 0 kudos

Resolved! STM32U575 - available pins for SPI / QSPI

 Hi @Issamos  Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)QSPI_CLK → PB2QSPI_NCS → PB6QSPI_IO0 → PD11QSPI_IO1 → PD12QSPI_IO2 → PE2QSPI_IO...

HA2375- by Associate II
  • 1331 Views
  • 8 replies
  • 2 kudos

Resolved! stm32H7 LTDC confusion

Hello, I want to use LTDC on the STM32H743VIT6 microcontroller, but when I enable this peripheral in CUBEMX, it does not activate correctly. For example, the pins for B are from B3-B7, while they should be from B0-B4, and the same goes for R, G.  

HOSI_0-1762926289188.png
HOSI by Associate
  • 419 Views
  • 1 replies
  • 0 kudos

Resolved! Can't flash the board (tried 3 different programmers)

Hello, I bought STM32H743XIH6 board and first tried to program it with FTDI programmer and STM32CubeProgrammer. It looks like the serial interface detects the board correctly as I can see it in the STM32CubeProgrammer but fails at a read attempt of 0...

Mondo by Associate
  • 998 Views
  • 4 replies
  • 1 kudos