STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f103c8t6

i have flashed a stm32f103c8t6 with freejoy code but now i am trying to re-use this for another project but how to i flash this back to a stock form. as when plugged back in to pc its coming up with they freejoy and not able to get it to show for pro...

caver99 by Associate
  • 2551 Views
  • 3 replies
  • 0 kudos

What is the maximum UART speed on the STM32H7B0xB?

I'm looking at the STM32H7B0xB. I'm confused about what the actual maximum baud rate of the UART (in asynchronous mode) is. I'm getting three conflicting answers:Section 3.38 (the USART section of the datasheet) says: "These interfaces provide asynch...

Resolved! Built In LED Stopped Working

Hello,I was using STM32 Blue Pill board and it was working fine until few hours ago. It suddenly stopped working. I was trying to make the built-in LED (At PC13) blink using Arduino IDE but it's not even blinking when i do Reset now. I've tried Flash...

STM32G051 ADC Calibration issue

Hi I am using the STM23G051C8T6 for the internal RTC and an external battery on Vbat. I noticed if I perform the Calibration using the following lineHAL_ADCEx_Calibration_Start(&hadc1);my initial ADC reading will be lower then actual reading. For exa...

KDham.1 by Associate II
  • 2168 Views
  • 3 replies
  • 0 kudos

I'm out before I even really got started...

Hopefully someone at STE cares enough to take this honest feedback on board...My project had to move from atmel to something with more performance.  I settled on STM32.The experience has been terrible due to sub-optimal documentation from STE, relyin...

Is HAL_I2C_GetState() required in polling IO mode?

I am using the HAL library with an STM32L07xx processor. To keep things simple, I have implemented master transfers on the I2C bus in the polling IO mode. Most of the time it seems to work, however once in a while a master transmit seems to get lost....

DavePfz by Associate III
  • 2770 Views
  • 1 replies
  • 0 kudos

Resolved! Generated PWM resolution

Hi,I am new to STM32 devices. I have a STM32F407 Discovery 1 board.I wanted to generate a 1 KHZ signal with a 50% duty cycle.The timer clock is configured to 84 MHZI am using TIM3 on channel 4. The prescaler is 210 and the counter period is 400 =>840...

2.png 1.png PXL_20231013_173821654.jpg
BAW by Associate III
  • 2085 Views
  • 1 replies
  • 2 kudos