STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Compatibility of different footprints of same MCU type

Hello,I want to change the MCU STM32F779AIY to STM32F779NIH6I already checked the pinout in CubeMX and i can use the same config for the peripherals at the same naming of pins (PB1, PA4 and so on).Do i need to change anything at the software if i cha...

Resolved! stm32f429-Disc1

What is the minimum and maximum voltage the internal ADC of stm32f429 can measure ?

harry123 by Senior II
  • 3955 Views
  • 7 replies
  • 2 kudos

STM fgets character limit

fgets ignores my limit and is trying to read 1024 characters.char *fgets( char *str, int numChars, FILE *stream );as I understand fgets it is supposed to read up to numCHars characters from stream into str. It should also stop on a newlineThe behavio...

Qye by Associate II
  • 2241 Views
  • 2 replies
  • 0 kudos

RTOF: Receiver timeout - UART

Hi,HAL Version used - 1.10.0I am using RTO interrupt to identify if the transmitter has finished sending a packet. In the IRQ handler "void HAL_UART_IRQHandler(UART_HandleTypeDef *huart)", this is considered as an error and it is aborting the ongoing...

Luke_abc_1-1696761236413.png
Luke_abc by Associate III
  • 5189 Views
  • 10 replies
  • 1 kudos

HAL_TIM_Base_Start_DMA

i did not find any example explain how i can get value counter from time by DMA in main programnote i use stm32g030f6#HAL_TIM_Base_Start_DMA/* USER CODE BEGIN Header *//**  *****************************************************************************...

STM32F446 VREF+ power up condition

Hello everyone,I am in the process of designing a PCB with an STM32F446ZET6 and I have a question regarding the voltage on the VREF+ pin. In the datasheet on p. 76, footnote 4 states that the condition "VDDA-VREF+ < 1.2 V" needs to be respected. Tabl...

mabe_rs by Associate II
  • 2459 Views
  • 2 replies
  • 1 kudos

I2S Peripheral - Disable slot swapping?

Hello,Is there a way to disable the slot swapping of the I2S peripheral?Take the following example, without any HAL_I2S callbacks... void start_loopback(I2S_HandleTypeDef* is2_handle) { printf("--> Starting algorithm loop back...\n"); for (int i=0...

GPRS Communication with STM32

Hi, I am using STM32F4 series controller or can even use any other controller series but i want to start using it for GPRS communication. How can i start using it for using Communication. Also how can i do API calling for certain strings using these ...

DJ17 by Associate II
  • 3517 Views
  • 5 replies
  • 0 kudos