*Using FP-AI-Vision1 Packimport the binary webcam, the screen is black.import the people detection binary, the screen is a mess.No camera picture.While import the Tutti Frutti demo, it can normally run.
Thanks!! I want to add this in my ai-vision project.It do image classification task now, and I want to add sending result through WIFI.(PC or mobile phone, only need text can be sent)I met some problem:The AT command seems to need ESP01 module conne...
I've commented in another questionFeed Detail (st.com)The best comment is from me, I've uploaded some pictures about this issue.(The default screen serial num is A225300780 with a QR code on right.The new screen is A214500023 without QR code.)
Yes. A03 or 01,02 doesn't matter, they're both A03.The default screen serial num is A225300780 with a QR code on right.The new screen is A214500023 without QR code.
Hey Guys, GOOD NEWS!It's the screen hardware problem, I bought a separate screen (B-LCD40-DSI1 4" WVGA TFT LCD) from mouser, which is same type but can normally display.↓ difference between default screen and separate screen↓ package of screen modu...