cancel
Showing results for 
Search instead for 
Did you mean: 

Failed to get BIC code for P-L496G-CELL02 ESIM activation

XYang.3
Associate II

I follow the instructions on "How to enable SIM MFF2 connectivity with P-L496G-CELL02.txt" from the link of "https://www.st.com/en/evaluation-tools/p-l496g-cell02.html#tools-software" utilities section.

The device was configured and actived ESIM, after that, tried to get BIC code, however, got negative response, as shown in the following:

I tried 2 P-L496G-CELL02, both gave the same results. Please help...

1. Type In "at at<CR>", got the expected response:

ATParser:*** SEND (size=3) ***
at<CR>
<CR><LF>
OK<CR><LF>
2, type in "at ati<CR>"
ATParser:*** SEND (size=4) ***
ati<CR>
<CR><LF>
Quectel<CR><LF>
BG96<CR><LF>
Revision: BG96MAR02A08M1G<CR><LF>
<CR><LF>
OK<CR><LF>
3. Type In "at AT+CRSM=176,12275,0,0,16,,"3F00"<CR>", however, got negative response.
ATParser:*** SEND (size=33) ***
AT+CRSM=176,12275,0,0,16,,"3F00"<CR>
<CR><LF>
+CME ERROR: unknown<CR><LF>
ATCore ERROR:AT_sendcmd error
ATCore ERROR:AT_sendcmd error: parse from rsp
LOG ERROR #1: channel=2 / errorId=11 / gravity=2
LOG ERROR #2: channel=2 / errorId=14 / gravity=2
CS ERROR:<Cellular_Service> error when sending direct cmd

AT+CRSM=176,12275,0,0,16,,"3F00" command FAIL

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0