cancel
Showing results for 
Search instead for 
Did you mean: 

Cleaning after reflow: STM32L151VC6 UFBGA100 package

geigerm
Associate

Hallo, I have a question for the STM32L151 in the UFGBA100 package.

There is a technical note  for the WLCSP-package existing (TN1163). In this note it is not recommended to clean the WLCSP package and also apply no ultrasonic cleaning methods.

We are using the UFBGA100 package. I cannot find any recommendations for this package how to clean them on an assembled board. In the application note AN2639 reflow recommendations are given and in figure 1 there is a hint for cleaning, but no further details are given.

As I suspect the UFBGA100 is similar to the WLCSP package in case of size, balling and construction.

Does anyone has experience or see a risk of cleaning the UFBGA100 package in ultrasonic processes?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0