STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 DFP 3.1.1 spi issue

Hiwe are working with a STM32H7 project. Recently we upgrade the packages and the Keil.STM32H7xx_DFP.2.5.0 grow up to DFP 3.1.1.Since the upgrading, the SPI start to fail (some data bits were wrong in every reading). Downgrading to DFP 2.5.0 it works...

Main Flash memory endurance

Hi Team i have one doubt i am using stm32wle5cc controller and  stm32wle5cc controller have 256Kb flash memory and each page is 2Kb. and  stm32wle5cc controller  flash memory support  10k cycles write operations after completes 10k write operations w...

kRaje.1 by Associate II
  • 7677 Views
  • 7 replies
  • 1 kudos

Resolved! Enabling instruction prefetch in the HAL (potential bug)

Hello,According to the reference manual RM0456 7.3.3:"Prefetch is enabled by setting PRFTEN in FLASH_ACR.PRFTEN must be set only if at least one wait state is needed to access the flash memory" Compared to that I've seen that in the U5 HAL, in the fu...

GG.2 by Associate II
  • 4475 Views
  • 5 replies
  • 0 kudos

TIM1 connected to a comparator with Falling Edge event

 We are trying to configure TIM1 and an internal comparator to turn-off the TIM1 complimentary PWM outputs on a falling edge event and generate a TIM1 break interrupt.I was successful to do this with a comparator with Rising Edge event.But when TIM1 ...

bolurian by Associate II
  • 1152 Views
  • 0 replies
  • 0 kudos

Resolved! CAN Communication U5A5ZJ-Q

Hello It's been days now that I'm trying to work with the CAN Communication on the U5A5ZJ-Q. I couldn't find any documentation on it (aside from the FDCAN), Hence, I would like to get some documentation on the board since there are CAN Tx and CAN Rx ...

lfresnay by Associate II
  • 1187 Views
  • 1 replies
  • 0 kudos

STM32F429 Disc1 LED5 (Vbus pin is working)

Hello guys, I have an issue that when I program the board, LED5(it says Vbus LED) is lighting. (it is green) Datasheet of the board hasn't got a info or i cant see any info about that.Could you help me with this issue ? Thank you...

Resolved! Can I use an Stlink of a Nucleo-mini board to program another ?

I have a Nucleo-l432kc board that I actually fried by accident touching one of the pins with my power supply probes while they shared the same ground during a risky test of mine anyway the problem now is I can't find a replacement at the moment in my...

Susano by Associate II
  • 1360 Views
  • 1 replies
  • 2 kudos

Resolved! STM32 MSI (MSIK) PLL Mode/Auto Calibration: Frequency Error

I have a STM32U595 with a 32.768kHz LSE oscillator.I wish to generate a 1ms/1kHz timebase with the accuracy/drift characteristics of the LSE, so naturally I went to make use of the "Hardware auto calibration with LSE (PLL-mode)" feature.Firstly, can ...

BCowp.1 by Associate II
  • 4290 Views
  • 3 replies
  • 0 kudos

MOBUS TCP - is there any library to work with ?

Hello eveyone,I'm trying to communicate with MODBUS TCP between a STM32 Nucleo-F429ZI board and a PLC. There is a LAN8742A transceiver on the board, do you know any modbus TCP library that is compliant with ?Thanks in advance for you time

AKrie.4 by Associate
  • 6671 Views
  • 7 replies
  • 4 kudos