STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103CBT6 Driving PWM for Synchronous DC/DC Buck Converter

Hi,I am quite new to STM32 MCU family and have a quick question. I attached schematic for the reference. Is STM32F103CBT6 capable of driving complementary 50 kHz of PWM signals(HI and LO) with configurable duty cycle for the gate driver IC? Yes, I am...

shin212 by Associate II
  • 3082 Views
  • 1 replies
  • 0 kudos

Maximum analog output voltage from STM32H723ZG

Hi, which is the maximum analog output voltage from the STM32H723ZG? In the datasheet I saw that there are two Op-Amp inside the MCU with gain from 2 to 16. How can I use this Op-Amp? I have to do something about the hardware or I have just to write ...

ECiot.1 by Associate II
  • 3293 Views
  • 5 replies
  • 0 kudos

Resolved! Documentation: USART1/2 and APB2/1 on STM32U5 series

Is USART1 on APB1 (AN5593, tab.17) or APB2 (DS, RM, CubeMX) and USART2 on APB1 (DS, RM, CubeMX) or APB2 (AN5593, tab.17)? Guess, there is an issue in an5593-how-to-use-the-gpdma-for-stm32u5-series-microcontrollers-stmicroelectronics Rv.4 , isn‘t it?

FB1 by Associate II
  • 2077 Views
  • 2 replies
  • 0 kudos

driverchip for GPIO support

Hello forum,I need some hardware help to modify my PCB, which was developed by other people.I use STM32F103. I have one "Master"-Board and several "Slave"-Boards (up to 20) with same controller.Because of current saving reasons I need to set the cont...

APlöt.1 by Associate II
  • 3573 Views
  • 6 replies
  • 1 kudos

ST-Link's Mass storage file write from firmware application

Hello everyone,i would like to know if it would be possible to write data on the STLINK mass storage device from the firmware application. This would be really awesome for debugging, logging, testing, etc.I am only aware of dragAndDrop programming fe...

jboui.1 by Associate II
  • 3356 Views
  • 5 replies
  • 0 kudos

Resolved! USART6_CTS pin of STM32F407

Hello forum and devs!Have one simple question: datasheet of STM32F407ZGT (STM32F40x series) and Cube MX says me, that this MCU doesn't contain USART6_CTS pin, but contain two USART6_CK pins. Is it mistake, and where is USART6_CTS pin?Official datashe...

Powerjack_0-1698399674722.png

NiPdAu plating looks like copper finish

We have received   STMICROELECTRONICS SPC58EG80E5QEC0X, the Terminal Plating is Nickel/Palladium/Gold (Ni/Pd/Au), we see that the terminals look copper finish

JKF by Associate
  • 992 Views
  • 0 replies
  • 0 kudos