2023-06-08 9:09 AM
On STM32G491 (and family) MCUs the on-board temperature sensor can be read by ADC1 or ADC5 to provide junction temperature.
RM0440 Rev 7 informs us:
In order to read the temperature sensor we must "wake" it from power-down mode by setting the VSENSESEL bit in the ADCx_CCR register. Two such registers exist which I assume to be: ADC12_CCR and ADC345_CCR.
I cannot find any documentation on how to do this and there does not seem to be any example projects.
How to enable this bit please?
2023-06-08 9:37 AM
ADC12_COMMON->CCR |= ADC_CCR_VSENSESEL;
ADC345_COMMON->CCR |= ADC_CCR_VSENSESEL;
JW
2023-06-08 9:59 AM
That is what I thought, but no! My raw read values are still nonsense.
My ADC config code (from STM config tool)
static void MX_ADC5_Init(void)
{
/* USER CODE BEGIN ADC5_Init 0 */
/* USER CODE END ADC5_Init 0 */
/* USER CODE BEGIN ADC5_Init 1 */
/* USER CODE END ADC5_Init 1 */
/** Common config
*/
hadc5.Instance = ADC5;
hadc5.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV8;
hadc5.Init.Resolution = ADC_RESOLUTION_12B;
hadc5.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc5.Init.GainCompensation = 0;
hadc5.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc5.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc5.Init.LowPowerAutoWait = DISABLE;
hadc5.Init.ContinuousConvMode = DISABLE;
hadc5.Init.NbrOfConversion = 1;
hadc5.Init.DiscontinuousConvMode = DISABLE;
hadc5.Init.DMAContinuousRequests = DISABLE;
hadc5.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc5.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc5) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC5_Init 2 */
/* USER CODE END ADC5_Init 2 */
}This is how I trigger a read (every 1-second)
/* Trigger MCU Temp ADC read */
ADC345_COMMON->CCR |= ADC_CCR_VSENSESEL;
HAL_ADC_Start_IT(&hadc5);Then I save the raw value in my IRQ handler
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef * hadc) {
/* MCU temperature */
TempValue = HAL_ADC_GetValue(&hadc5);
}The resulting TempValue is either 0, 1 or 2.