STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H723VG using Timer outputs as GPIO Output

Hi community!I have a STM32H723VG and I use Timer1 on that device to generate complementary PWM Outputs (Chx + ChxN) on channel 1-3 plus a 1-channel PWM on Channel 4. When the PWM is not needed, I have to set the output pins of the timer either high ...

CBerg by Senior II
  • 3036 Views
  • 1 replies
  • 0 kudos

STM32C011 System/Open Bootloader

Hello,I'm using an STM32C011 for a product we are developing, and I want to use ST's default System/OpenBootloader (via UART) that the virgin chips have on board. That way in production we don't have to download our custom bootloader, and we'll use t...

starivore by Associate II
  • 6989 Views
  • 8 replies
  • 5 kudos

32H563Zi can't work in VDD=1.8V?

Hi, Sir: Currently using H563ZI (MB1404C) to develop programs.When VDD=3.3V, MCU works normallyWhen VDD=1.8V, the MCU functions abnormally (USB function fail), but the specification indicates that it can support VDD=1.8V. Where should I set this on t...

Charles63 by Associate II
  • 1924 Views
  • 3 replies
  • 0 kudos

CRS SYNC setup with LSE and CubeMX puzzle

I try to setup CRS SYNC setup with LSE using the latest CubeMX.It appears that when CRS SYNC with Source LSE is selected, LSE does not get initialized unless RTC is active as well and its clock source is set to LSE. E.g crystal drive level option doe...

RCC-A.png RCC-B.png RCC-C.png
TDJ by Lead
  • 3275 Views
  • 2 replies
  • 3 kudos

Compatible SDIO voltage translator for STM32F413

Hi,We are designing STM32F413ZHJ6 at 1.8V and are looking for a suitable level translator to 3.3V for the on-board microSD connector. I'm considering NXS0506UP or NVT4858. Just wondering if these parts would be compatible with the STM32? Any suggesti...

Thai by Associate
  • 2542 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H5 Need bootloader pins

As per errors in AN2606 and this thread https://community.st.com/t5/stm32-mcus-products/stm32h5-bootloader-uses-usart-pins-that-do-not-match-roles-in/m-p/594610#M224078 I need the correct pins that STM32H563/STM32H573 use for USART1/2/3 and FD-CAN bo...

MBC by Associate III
  • 5949 Views
  • 6 replies
  • 3 kudos

measure power consumption of STM32F769I-DISCO

i want to measure the power consumption of my stm32f769 discovery board, while its runs a simple NN model. Is there any way to do it using the STMCubeMX? or do i need to get a X-NUCLEO-LPM01A power shield? If so, would that be compatible with the STM...

aben118 by Associate II
  • 2041 Views
  • 1 replies
  • 0 kudos