Skip to main content
BRIAN_LAI
Associate II
July 4, 2023
Solved

STM32H503RB I3C Target TX-FIFO Size Question

  • July 4, 2023
  • 6 replies
  • 8454 views

I am using NUCLEO-H503RB as I3C Target with LL library.
What's the minimum size of TX-FIFO available when I3C Target is reading by Controller?
I setup I3C Target TX-FIFO using function "LL_I3C_ConfigTxPreload" with 1 byte, but it always runs 8 bytes per time.

According to the datasheet, the size of TX-FIFO would be TGTTDCNT if size is lower than 8 bytes.
Tx-FIFOTx-FIFO

My TGTTDCNT settings:
TGTTDCNTTGTTDCNT

The test procedure is I3C Controller start a private read with 11 bytes and Target return the array contents.
The source code is attached, the result diagram is described below.
I3C Read TestI3C Read Test

This topic has been closed for replies.
Best answer by Foued_KH

Hello @BRIAN_LAI , 

The minimum size of TX-FIFO available when I3C Target is reading by Controller is 1 byte.
You need to indicate the status of TX FIFO preload (target mode) by using : LL_I3C_IsActiveTxPreload. Then you can Set TX FIFO Preload (target mode) LL_I3C_ConfigTxPreload

Foued

6 replies

Foued_KH
Foued_KHBest answer
ST Employee
July 4, 2023

Hello @BRIAN_LAI , 

The minimum size of TX-FIFO available when I3C Target is reading by Controller is 1 byte.
You need to indicate the status of TX FIFO preload (target mode) by using : LL_I3C_IsActiveTxPreload. Then you can Set TX FIFO Preload (target mode) LL_I3C_ConfigTxPreload

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BRIAN_LAI
BRIAN_LAIAuthor
Associate II
July 5, 2023

Hi @Foued_KH ,

I think the root cause may be the Target Interrupt "I3C_EVR_TXFNFF" trigger when TX-FIFO is not full with 8 bytes.
Is it required to fill TX-FIFO full every time before I3C Target being read from Controller?
Are we able to implement I3C Target with using TX-FIFO only a single byte?

Foued_KH
ST Employee
July 5, 2023

Hello @BRIAN_LAI , 
Just configure Tx Fifo Threshold : 1 byte 

/** Configure FIFO**/
sFifoConfig.TxFifoThreshold =HAL_I3C_TXFIFO_THRESHOLD_1_4;

Foued

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
BRIAN_LAI
BRIAN_LAIAuthor
Associate II
July 5, 2023

Hi @Foued_KH ,

I've already setup with "I3C_TXFIFO_THRESHOLD_1_4".
TX_FIFO_Config.png

The interrupt condition is "One or more free space available in TX-FIFO". (1 byte empty then trigger Interrupt)
Is it possible to change the interrupt condition to "TX-FIFO empty" ? (only trigger Interrupt when 8 bytes empty)

Trigger.png

Foued_KH
ST Employee
July 5, 2023

Are you sure that you are sharing the target code ?
because I see the process for the dynamic addressing in the target side 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.