Dear community, Since i have travel inside parameters, now at each compilation, a file " Startup_stm32f103rgtx.s" is opening...Close this files, it's come again.Do you have an idea to disable/ hide it ?
Dear communityI develop a 'robot" with odometrie.Each geared DC motor have a rotary magnetic encoder for speed regulation.My question is about avoid count overload.I use a timer for read encoder count. Each interrupt, i print the value.My aim is avoi...
Dear community,I work on a 'robot' with odometrie.Each geared DC motor have a rotarty magnetic encoder ( AS5047P).I use Quadrature Output to Encoder mode. It's works but i have some questions...> get_valueWhathever the configuration on STMCube, the v...
Dear everyone,I'm trying to manage a DC motor with IC controller in PWM.My frequency have been calculated for have 12bits resolutions (Fclk :72Mhz > Fpwm17.5Khz). TIM2->CCR1 = 30;
HAL_TIM_PWM_Start(&htim2, TIM_CHANNEL_1);
HAL_GPIO_WritePin(GPIOB, MA_...
Thanks for you reply.The 17,5Khz have been choosed for three raison:> Current pulse smaller> Sound not audible> 12bits resolution as calcul with the formula.I will test it now!
You have right, my problem is not a bug from STM32 but a C acknowledge issue.I'm not a complete newbie and i have all documentation next me... the transition from theory to practice is not always easy.My data is store like that :uint8_t command[10]={...
Ok, i have found !So in your mainextern UART_HandleTypeDef huart1;instead of "UART_HandleTypeDef huart1; "AND in your other file, add UART_HandleTypeDef huart1;