Skip to main content
MPetr.3
Associate II
March 3, 2021
Question

Low Power Mode StandBy at STM32L562 - SRAM2 Data retention cannot be disabled

  • March 3, 2021
  • 3 replies
  • 4356 views

Hello Community,

I am programming the STM32L562E-DK discovery board and working with the Standby low-power mode. In the data sheet there are 3 standby variations explained:

  • Standby with Full SRAM2 data retention
  • Standby with 4kB SRAM2 data retention
  • Standby without any data retention (all SRAM1 and SRAM2 is lost)

I cannot reach the variations, where part of the SRAM2 or all SRAM2 data retention should be disabled.

Always after I wake up the processor from the standby mode the data in SRAM2 is still there. SRAM1 is lost (which is correct).

I have tried everything to activate the Standby mode without any data retention, but it doesnt work.

To put the processor in standby mode I use the following code:

__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_SB);
if (__HAL_PWR_GET_FLAG(PWR_FLAG_WUF2) != RESET)/* Check and Clear the Wakeup flag */
{
	__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);
}
HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2_HIGH);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);
HAL_PWREx_EnableUltraLowPowerMode();
HAL_PWREx_DisableSRAM2ContentRetention();
HAL_PWR_EnterSTANDBYMode();

I checked every important register, especially the PWR->CR3->RRS bits which determine SRAM2 data retention.

My code is pretty much based on the official standby mode example at https://github.com/STMicroelectronics/STM32CubeL5/blob/master/Projects/STM32L562E-DK/Examples/PWR/PWR_STANDBY/Src/main.c .

I don't know if I am missing an instruction or if there exists a hardware bug which leads to the disability to disable SRAM2.

If anyone can help I would very much appreciate it.

Thanks in advance.

This topic has been closed for replies.

3 replies

Mike_ST
ST Technical Moderator
March 3, 2021

Please check L5x2 errata stheet :

https://www.st.com/en/microcontrollers-microprocessors/stm32l5x2.html#documentation

There is one item talking about SRAM2 and standby, but I didn't check if it matches your case.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
MPetr.3
MPetr.3Author
Associate II
March 4, 2021

Thank you for your answere Mike.

I have checked the errata sheet but sadly this is not the case.

It says :

Since I am directly transitioning from run mode to standby "with" modes, I don think this errata is valid for my case.

I am still looking for a solution.

MLint.1
Associate II
July 15, 2023

I have seen this too. Ie, SRAM2 data being retained when the RRS bits are clear. i read them back to check. What bought me here is the converse,  and for me, a very serious problem. The RRS bits are set for 4 k SRAM2 retention, and after a period of weeks or months, the product is acting as though SRAM2 data retention through standby has failed, SRAM2 being filled with pseudo random garbage on wake from standby.