User Activity

Cant program STM32G031J4 with stm32CubeProgrammer 2.16.0 (bootloader 3.1). It display default flash size of 63Kb and all command have errors ( erase/read/write.....). 
Spoiler  Hi, I have a question about the size of the flash of STM32G0J6. When i use STM32 cube programmer - CLI i saw that the size of the flash of the STM32G0J6 is 64Kb. I try to write everywhere in this memory it works. The datasheet say that the S...
Hi, I found a bug in stm32cubeProgrammer version v2.13.1. When you try to readout unprotect an STM32H7A (without smps) and if its rdp level is set to 1, that didn't works. I have to unlock it manually inside my software.  
Hi, I made an asm soft for the H5 (works well with H7,G4,G0,F7,F4,F0). That software configure the stm32H5 into an USB CDC device. When my frequency of my main clock, apb1 and apb2 is below 220 MHz, my software works well but when i put my main clock...
i have fuse 1.1.2 version and full_ble stack in the m0. The option bytes are 0x1FFF8078=0x9E2BD000 and IPCCDBA = 0.when i start the m0 ( bit 15 of PWR_CR4) I have that in the SRAM2B 20030000 : 24 00 03 20 00 00 00 00 00 00 00 00 00 00 00 0020030010 :...
Kudos given to