STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32N6570-DK boot from external flash error

Hello,I’m working with an STM32N6570-DK, and I’m trying to run a very simple LED-blinking application as part of the FSBL.When I debug the project using STM32CubeIDE, everything works correctly and the LED blinks as expected.Next, I want to flash the...

lou_v by Associate II
  • 1357 Views
  • 9 replies
  • 1 kudos

Resolved! STM32L476 vs STM32F411 vs STM32F303

Good morning.I'm still trying to develop in STM code.I have an open-source code developed for the STM32L476.Questions:If I generate a compiled HEX for the STM32L476, will it run on the 411?Are they compatible?Is it possible to migrate to an STMF303 o...

MIPI Camera on STM32N6

Hi everyone,I'm working on a project with an AR0144 image sensor connected to CSI2. (STM32N6)I have a question: if I use PIPE0 without any ISP processing of ROW10 data from the sensor to memory, do I still need to use ISP?Do I need to initialize it? ...

STM32N6 is only flashable after POR

Hi,We have a weired problem with a custom N657 design.When using the Nucleo board, its possible to flash the program on the external flash, as long as BOOT1=1.The programmer resets the board and it flashes the firmware normally every time.On our boar...