Skip to main content
Associate III
Apr 25, 2025 2:30 PM UTC
Solved

CAN in Normal Mode with STM32F407 microcontroller

Hello everyone,

I'm trying to switch from loopback mode to normal mode. So the program is working perfectly in loopback mode but i had to adapt it so i can use it in the desired normal mode.

I switched to the HSE as a source clock for CAN communication and I'm using PB8 and PB9 for CAN_Tx/Rx.

As a transceiver I'm using the SN65HVD230 with a 120 Ohm terminating resistor and the CANH and CANL are wired correctly to an DB9 connector then to a CAN interface for analyzing.

- I also checked the baud rate and i made sure that there's no mismatch.

- I selected the right channel for the CAN interface

- The transceiver is connected to VDD and GND

- The acceptance filter is configured to let any frame pass through it

- The interruption in the RX is enabled

- The error I'm receiving is an acknowledgment error from the CAN interface

You can find attached my project and i hope you can help me.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 25, 2025 2:45 PM UTC

Hello,


@Azizz wrote:

I switched to the HSE as a source clock for CAN communication and I'm using PB8 and PB9 for CAN_Tx/Rx.

As a transceiver I'm using the SN65HVD230 with a 120 Ohm terminating resistor and the CANH and CANL are wired correctly to an DB9 connector then to a CAN interface for analyzing.


Hello,

1- Need to provide more details about the hardware: what board are you using? a sketch to show a complete CAN bus your bard containing the F4 MCU + the transceiver + the CAN bus + the second CAN node (you said CAN interface for analyzing). You need to give details about that "CAN interface for analyzing".

2- Also did you pull the Rs pin of the transceiver down (connected to the GND)?

mALLEm_0-1745592221912.png

The hardware must be 100% OK to establish a good CAN communication.

3- Also please remove the pull-up resistor on the Rx pin:

mALLEm_1-1745592312936.png

4- Please make a photo of your complete setup.

5- I didn't see the declaration of the Rx FIFO0 nor FIFO1 callback in your code:

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *CanHandle)
void HAL_CAN_RxFifo1MsgPendingCallback(CAN_HandleTypeDef *CanHandle)
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 25, 2025 2:45 PM UTC

Hello,


@Azizz wrote:

I switched to the HSE as a source clock for CAN communication and I'm using PB8 and PB9 for CAN_Tx/Rx.

As a transceiver I'm using the SN65HVD230 with a 120 Ohm terminating resistor and the CANH and CANL are wired correctly to an DB9 connector then to a CAN interface for analyzing.


Hello,

1- Need to provide more details about the hardware: what board are you using? a sketch to show a complete CAN bus your bard containing the F4 MCU + the transceiver + the CAN bus + the second CAN node (you said CAN interface for analyzing). You need to give details about that "CAN interface for analyzing".

2- Also did you pull the Rs pin of the transceiver down (connected to the GND)?

mALLEm_0-1745592221912.png

The hardware must be 100% OK to establish a good CAN communication.

3- Also please remove the pull-up resistor on the Rx pin:

mALLEm_1-1745592312936.png

4- Please make a photo of your complete setup.

5- I didn't see the declaration of the Rx FIFO0 nor FIFO1 callback in your code:

void HAL_CAN_RxFifo0MsgPendingCallback(CAN_HandleTypeDef *CanHandle)
void HAL_CAN_RxFifo1MsgPendingCallback(CAN_HandleTypeDef *CanHandle)
To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.