STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G4 MCU peripheral Not working except JTAG and Power Pin

Dear Community member,We have developed a PCB for Air pollution measurement using STM32G473VET6 MCU. We were able to flash the program successfully, but we didn't receive any output from GPIO, UART, USB, etc. None of the peripherals are working excep...

Neeraj by Associate II
  • 1796 Views
  • 2 replies
  • 0 kudos

Resolved! CAN Normal Mode Communication between 2 boards

Hello, I am trying to implement a Normal Mode CAN communication using the STM32F407 discovery board and sn65hvd230 transceiver. It works fine for Loopback mode but when I change to Normal mode I get a Bit Dominant error. I am setting the bit rate to ...

STM32F405 vs STM32G4

Hi ST experts,Does STM32G4 series MCU support Vocoder feature? If yes, do you have any related documents available for reference? Current design is using STM32F405 which can support Vocoder application. Thanks. 

STLearner by Associate III
  • 3570 Views
  • 2 replies
  • 0 kudos

Resolved! stm32 HAL Library

Hi Everyone,                    Can i use the HAL based library in my code for making commercial product?                    or                   Need to use only register based code for making commercial products?

Resolved! STM32 F4 CANBUS communication issue

Hello, I am trying to program Can Bus protocol with two stm32 boards. I used MCP2551 and VP230 can transiciever but both of them doesnt work or my code doesnt work I dont know. I am programming normal mode. My purpose is when press the any button of ...

maZers by Associate III
  • 11540 Views
  • 8 replies
  • 2 kudos

Resolved! How to reduce power consumption while connected via CDC USB

I'm developing a board with an STM32L452 and would like to find out if I can improve power consumption while it remains connected via USB (as a device). I've tried putting the device to sleep using the following code: while (1) { // ... do stuff HA...

antfarmer by Associate III
  • 6835 Views
  • 10 replies
  • 4 kudos

Sending message from slave to master (SPI)

Hello,I'm trying to send a message from slave to master using spi (I'm using only one stm board) and so far nothing I tried has worked. AFAIK for the slave to send data to master, the master has to initiate communication first by sending clock signal...

Jordalic by Associate II
  • 5361 Views
  • 4 replies
  • 0 kudos

Unable to access QuadSPI Flash 2 with stm32h747i

Hi im currently using STM32H747I EVK board and working on QSPI ,im able to perform all the QSPI operations in FLASH1 but when u configure it as the FLASH2 nothing works . static void MX_QUADSPI_Init(void){ /* USER CODE BEGIN QUADSPI_Init 0 */ /* USER...

SPI + I2C Example Project

Hi, I am struggling to get SPI and I2C to work at the same time on my project I have tried multiple things (DMA, interrupts etc...) are there any example projects that already have this implemented? I am simply trying to read an I2C sensor value and ...

Linkpad by Associate III
  • 2271 Views
  • 3 replies
  • 2 kudos