cancel
Showing results for 
Search instead for 
Did you mean: 

STM32l496: Clocking timer using LSCO

HZaib.1
Associate III

Hi, I wanted to clock my timer output using LSE crystal, but unfortunately only tim2 is supported with this feature. 

But then I saw an option of LSCO as output in cubemx, this enables the pin on MCU and according to documentation this output LSE clock on that pin. So I was thinking about routing this signal to timer input as timer is going to be configured in ETR mode. So my question here is has anyone tried it and does it work ? is it even possible to route LSCO to multiple timer inputs ? 

 

I cant test it as I dont have a dev kit on my hand and only a custom board. 

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Andrew Neil
Super User

What chip are you actually using?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

stm32l496

So why have you tagged 7 other families too?

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

to reach every audience, as I guess this feature is also available in other series as well