STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Programming STM32L w/J-Link Compact

I have created the below circuit and build a PCBA. I'm using the J-Link Base Compact and Tag-Connect TC2030.Using the Arduino IDE I created a simple sketch to drive the 4 LEDs shown on the schematic below and blink every second.The code compiles ok a...

LEDTest.png

SPI TX DMA Request on Timer Update Event (STM32H7R)

Hello! I'm having issues having a successful configuration for the setup I need: an SPI TX transaction shall occur through DMA once a timer has reached its overflow count. The timer is then reloaded and proceeds to do cyclical SPI TX transactions. I ...

JCori by Associate III
  • 60 Views
  • 2 replies
  • 0 kudos

STM32F405RGT6 and STM32H743VGT6 FIT rates (MTBF)

Dear ST Support Team,I am working on a reliability calculation for an industrial hardware design. I need the official failure rate data for the following components:STM32F405RGT6: FIT rates or MTBF, and failure mode or FMECA report.STM32H743VGT6:  FI...

attestation roots for stm32 U3C5

Hi, I have a NUCLEO-U3C5ZI-Q board, and I'm trying to follow the DUA_USER attestation process.   I noticed that the existing Root CA certificates like here https://github.com/STMicroelectronics/STM32CubeU3/blob/main/Utilities/Certificates/ do not ver...

STM32H743VGT6 flash memory

Hi, I have bought STM32H743VGT6 and want to make bootloader and application. The issue is that its memory layout is confusing. In documentation and generated application I see/assume flash memory is:0x8000000 size 0x80000 (512kb bank1?) // bootloader...

JBond.1 by Senior II
  • 189 Views
  • 7 replies
  • 4 kudos