cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to sink 5V over USB PD

Nv7
Associate III

I am using an STM32G4 microcontroller with UCPD and the USBPD middleware. I was following this tutorial (same as AN5418 https://www.st.com/resource/en/application_note/dm00663511-how-to-build-a-simple-usbpd-sink-application-with-stm32cubemx-stmicroelectronics.pdf:(

https://youtu.be/-vsJhNIaHxE?si=3wosMAMXrO40mVZr

I, however, have a custom PCB without a TCPP chip, I'm not sure if this makes a difference. I set up everything according to the tutorial and I added the code it requires. Additionally, I added the following code to EvaluateSinkCapabilites: 

void USBPD_DPM_SNK_EvaluateCapabilities(uint8_t PortNum, uint32_t *PtrRequestData, USBPD_CORE_PDO_Type_TypeDef *PtrPowerObjectType)
{
/* USER CODE BEGIN USBPD_DPM_SNK_EvaluateCapabilities */


 USBPD_SNKRDO_TypeDef rdo;
 rdo.d32 = 0;
 /* Prepare the requested pdo */
 rdo.FixedVariableRDO.ObjectPosition = 1;
 rdo.FixedVariableRDO.OperatingCurrentIn10mAunits = 50;
 rdo.FixedVariableRDO.MaxOperatingCurrent10mAunits = 50;
 rdo.FixedVariableRDO.CapabilityMismatch = 0;

 *PtrPowerObjectType = USBPD_CORE_PDO_TYPE_FIXED;
 *PtrRequestData = rdo.d32;

 //USBPD_HandleTypeDef *pdhandle = &DPM_Params[PortNum];
 uint32_t size;
 uint32_t snkpdolist[USBPD_MAX_NB_PDO];  // Array to store sink PDOs
 USBPD_PDO_TypeDef pdo;

 // Get the list of sink PDOs
 USBPD_PWR_IF_GetPortPDOs(PortNum, USBPD_CORE_DATATYPE_SNK_PDO, (uint8_t *)snkpdolist, &size);
 HAL_Delay(100);

 ssd1306_Display(1);
 ssd1306_Fill(Black);
 ssd1306_SetCursor(0, 0);
 ssd1306_WriteString("Available PDOs:", Font_11x18, White);

 // Iterate through each sink PDO and print its details
 for (uint32_t i = 0; i < size; i++)
 {
	 pdo.d32 = snkpdolist[i];  // Get each PDO
	 char pdo_info[256];  // Adjust the size if needed
	 snprintf(pdo_info, sizeof(pdo_info), "%u mV, %u mA", pdo.SNKFixedPDO.VoltageIn50mVunits*50, pdo.SNKFixedPDO.OperationalCurrentIn10mAunits * 10);
	 ssd1306_SetCursor(0, 7 + i*7);
	 ssd1306_WriteString(pdo_info, Font_11x18, White);
 }
 ssd1306_UpdateScreen();

/* USER CODE END USBPD_DPM_SNK_EvaluateCapabilities */
}

I also have some code to manipulate the display in main() which is why I know the microcontroller is working. On a USB-A to USB-C cable nothing is changed on the screen, which means this function isn't getting called and its just getting 5V because its USB-A. On a USB C power supply it doesn't even turn on (no voltage is given), so I don't think this function is getting called or the negotiation is working at all, even though I've connected the UCPD CC lines to the port.

 

STM32CubeMx:

Nv7_0-1742192885965.png

 

I would greatly appreciate if someone helped me debug this!

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @Nv7 

I guess it's quite complex to follow your custom setup without testing it. I recommend using TCPP ports instead and x nucleo expansion board so that we can help you.

In general, the USB PD specification allows CC receiver (cReceiver) capacitance in the range of 200 pF to 600 pF.
For noise filtering purposes, an extra 390 pF +/- 10% capacitance must be added on each CC line close to the
TypeC connector.

When a TCPP0x is used, these capacitors must be added between the TCPP0x and the TypeC connector, as close to the Type-C connector as possible.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

10 REPLIES 10
FBL
ST Employee

Hi @Nv7 

I, however, have a custom PCB without a TCPP chip, I'm not sure if this makes a difference.

> Sure, it makes big difference. The issue could be linked to your hardware implementation. Double-check the schematic and PCB layout to confirm that UCPD CC lines are correctly connected to the USB-C connector on your custom PCB. Would you attach a trace .cpd ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Nv7
Associate III

Yes, the CC lines on the USB port are connected to the chip's UCPD CC lines, although I don't have any resistors on those lines just a direct connection - is that how it's supposed to work? I'm, not sure how to make a trace.cpd file.

FBL
ST Employee

Hi @Nv7 

I guess it's quite complex to follow your custom setup without testing it. I recommend using TCPP ports instead and x nucleo expansion board so that we can help you.

In general, the USB PD specification allows CC receiver (cReceiver) capacitance in the range of 200 pF to 600 pF.
For noise filtering purposes, an extra 390 pF +/- 10% capacitance must be added on each CC line close to the
TypeC connector.

When a TCPP0x is used, these capacitors must be added between the TCPP0x and the TypeC connector, as close to the Type-C connector as possible.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Nv7
Associate III

I picked the STM32 with the UCPD peripheral so that I wouldn't need to put an external USB-PD chip - if you still need an external chip why would you choose to use integrated UCPD peripheral instead of an external PD chip and a cheaper MCU?

FBL
ST Employee

Hi @Nv7 

TCPPs are designed to protect and enhance the USB Type-C/PD solution. They address the electrical challenges of implementing USB-C and USB-PD. 

  1. UCPD Peripheral:

    • Handles USB-PD communication like power negotiation.
    • Interfaces with the STM32 firmware stack for compliance with USB-PD policy management.
  2. TCPP Port Protection:

    • Protects the USB-C port from electrical issues like overvoltage, overcurrent..
    • Manages the power path by enabling or disabling VBUS, controlling external FETs.
    • Provides additional hardware support for specific USB-PD features like dead battery mode.

Using the STM32 UCPD peripheral alongside TCPP components provides a complete, robust, and cost-effective USB-C/PD solution. While the UCPD peripheral handles the protocol layer, TCPP components ensure physical protection and power path management

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Nv7
Associate III

Yes, but chips like the STUSB4500 exist and can do all of these functions for a low cost, so why would a customer get a chip with a UCPD peripheral? Am I missing some advantage that these chips offer versus a standalone chip?

FBL
ST Employee

Hi @Nv7 

As moderator, I suggest initiating a new discussion to address this query.

Developers can customize the USB Power Delivery application to integrate functionalities, like power role swap, GPIO signaling, and synchronization with other system components. This flexibility is particularly useful for some advanced configurations like supporting multiple PDOs (more than 3 PDOs) for both sink and source roles.

Also, such integrated solutions can enable the microcontroller's processing power and peripherals to handle USB PD tasks more efficiently without additional communication protocols like I²C ...

The robustness of the implementation depends on the quality of the developer's code. Alternatively, using the STUSB4500 ensures a robust solution through hardware-based functionality (auto-run mode).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
BoSt
Associate II

Hi!

I have the same setup and same problems. Using the STM32G431 without the TCPP chip.

Have you find any solution?

Thanks!  

Nv7
Associate III

I switched to the STUSB4500 and used the F072 instead which offers largely the same functionality, is roughly the same price, and actually works. I think the UCPD peripheral is meant for advanced users, its overkill for basic sink applications and unnecessarily complicated.