STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FDCAN repeated transmissions - CAN memory altered after TX ?

Heyho,question about FDCAN and repeating / timed transmission of the same messages:(this is neither about TT CAN nor auto re-transmission, but e.g. for messages which need to be sent every 100 ms repeatedly and "manually")After the first setting of t...

LCE by Principal II
  • 760 Views
  • 6 replies
  • 4 kudos

Bank switch does not always work

Hello everyone!I'm facing a problem when trying to switch a bank on STM32H745 MCU. The issue happens only when the debugger is disconnected. Our implementation uses the HAL library to perform Bank switch like this:HAL_FLASH_Unlock(); HAL_FLAS...

Core supply for STM32H573MIY3Q

Hello,we have to use the STM32H573 in the 80 Pin WLCSP with temperature Range 3 (to 125°C). So STM32H573MIY3Q was chosen. Due to a mistake we didn't recognized that the internal LDO can't be used. Now we have no space for placing additional component...

MarwinS by Associate
  • 418 Views
  • 1 replies
  • 0 kudos

STM32L432 nucleo I2C bootloader communication issues

Hello,I'm trying to test FW update over I2C using RPI as host and STM32L432 nucleo board as slave on port I2C1 which according AN2606 (table 152) should be available. I've connected 4.7k pullups on PA6 + PA7 pins and perform NRST to 0 and BOOT0 to 1 ...

MBeli.1 by Associate III
  • 623 Views
  • 4 replies
  • 0 kudos

Resolved! What is the best PLL configuration for H533 ?

Hi there,I'm starting to use the NUCLEO-H533RE board to evaluate the H5 device family.RM0481 has some errors on the PLL configuration:Fig.55 on page 461 shows a VCO range 0 between 128 and 560 MHz, but the description of bit 5 of register PLL1CFGR (p...

Kraal by Lead
  • 733 Views
  • 5 replies
  • 3 kudos

Resolved! STM32N6 H264 Video Encoder ASIC datasheet / manual

Hello folks,I am investigating the Video Encoder on the STM32N6 and have been working through the reference project (VENC_SDCard_ThreadX).The user manual (RM0486) is very vague on detailing the Video Encoder, and lists over 100 pages of registers whi...

exarian_0-1745948663250.png
exarian by Associate III
  • 3656 Views
  • 9 replies
  • 6 kudos