STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 USB host/device with USB-C connector

Hi, I want to use a USB with USB-C connector and STM32F427 mostly as a HOST for USB mass storage, but it has to be able to switch to device, works as serial port. A 5V can be applied to the USB by a power switch for a HOST mode, and can be detected w...

mkuczma by Associate
  • 2148 Views
  • 1 replies
  • 0 kudos

Resolved! Screen flickering while using TFT-LCD with LTDC

Hi.A custom board was built using the STM32H753XI. The board contains 16MB SDRAM and we want to use it with an LTDC to display a screen on a TFT-LCD.I used the embedded wizard to create the UI and verified that it displays correctly on the LCD screen...

LCD-Timing.png Clock.png

Using CubeIDE to configure I2S, can't set I2S Clock

hello, I'm tring to configure STM32F103RCT6 to interface a codec with I2S. I use a 8MHz external crystal as HSE, in the clock configuration page, the I2S clock is direct connect to SYSCLK and cannot be adjusted. the selected audio frequency is 48KHz,...

截屏2024-03-03 18.44.37.png 截屏2024-03-03 18.44.47.png
Wal by Associate II
  • 4314 Views
  • 5 replies
  • 0 kudos

Reg:Bootloader

Hello Team, I am trying to implement a bootloader for stm32f769 controller, My bootloader code resides in sector 0 and application code in sector 5. But I am not able to jump from bootloader code to application code. Any help will be highly useful. B...

LTDC MIPI-DSI Configuration using stm32H747 and ST7701S

Hi STM community, I have interfaced an st7701s driver IC-based display with stm32h747 chip using MIPI DSI in RGB565 mode and using only the internal SRAM(512KB) of stm32 as the frame buffer(2*480*480 Bytes) but the display framebuffer looks like star...

USB to CAN interface

Hello ST community, I'm working on an interface board based on STM32F412 to send CAN frame from a computer using USB communication. For the moment I'm doing some tests with the CDC stack and the default ST's USB virtual com port driver on Windows 10....

oli_the_true_one_0-1709195364993.png oli_the_true_one_1-1709195591831.png

Resolved! HSE crystal dead

HelloI am trying to powerup external 8MHZ crystal on STM32F407VET6 MCU but it is completely dead. I run the LED bliking program using HSI, and it is working sucussfully. Boot 0 and Boot1 pins have been PD with 500 ohm.  I also run the same code to us...

Nico3_0-1709283992146.png
Nico3 by Senior
  • 10422 Views
  • 20 replies
  • 10 kudos