cancel
Showing results for 
Search instead for 
Did you mean: 

AN4457-emulated-uart

JLee.21
Associate II

안녕.

HAL_UART_Emul_Receive_DMA 및 HAL_UART_Emul_Transmit_DMA를 사용하고 있습니다.

1Byte R/W를 시도 중입니다. stm32 go Error_Handler();

코드를 어떻게 변경해야 하나요?

 

감사합니다.

 

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
KDJEM.1
ST Employee

Hello @JLee.21 ,

Thanks to develop your posts in English so it helps us, and the users of our community understand your question and try to help you.

I've translated your question using a translation tool to increase the chances of getting you a reply from our experts and community members, since the majority interact in English.  

Here is the translation of your post using Google translate:

hi.

I am using HAL_UART_Emul_Receive_DMA and HAL_UART_Emul_Transmit_DMA.

Attempting 1Byte R/W. stm32 go Error_Handler();

How should I change my code?

Thank you.

 Are you using STSW-STM32156 example ?

Could you please give more details about your hardware? Are you using NUCLEO-F401RE boards?

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi, KDJEM1.

Yes, I'm using en.stsw-stm32156.zip.

I'm using stm32f4-discovery(stm32f401vct) board.

en.stsw-stm32156.zip code works very good, but it's receiving 2Byte adding last Byte 0x00 just write 1Byte.

So, How should i change code. also i want receive DMA using circuler mode.

Thank you.