User Activity

Using the CubeIDE Rev 1.12.1, I have loaded an application and set a breakpoint in an STM32L562 uC. I am using a Segger J-Link Plus probe (does the same with ST Link V2) to debug.  I know something has happened to the CPU from a code stand-point as t...
Here is the setup (Using timer 1 - 16 Mhz clock, counter = 3200) using OC channel to produce scope signal on output pin):void MX_TIM1_Init(void) {   /* USER CODE BEGIN TIM1_Init 0 */   /* USER CODE END TIM1_Init 0 */   TIM_ClockConfigTypeDef sC...
STM32Cube IDE w/ STM32L562QEIX part - generated a .IOC to match my hardware. Have a Sky High eMMC 8-bit part configured to use the eMMC/SD peripheral in 8-bit mode. Also using FS USB CDC as another large peripheral. I can program/debug the chip wi...
Using an STM32L562Q part: configured the clock tree to use LSI, MSI, and HSI48 internal clocks. Odd that RCC_OscInitStruct.OscillatorType = 0x3CCode generator is setting RCC_OSCILLATORTYPE_LSE as one of clocks to init but I don't have an external L...
New project with STM32CubeIDE version 1.10.01 Part is STM32L562QConfigured chip, running bare metal (no RTOS). SysTick source is TIM2.main() -> HAL_Init() -> HAL_InitTick -> HAL_TIM_Base_Start_IT()Then, right after the TIM2 is enabled, we get <signa...