cancel
Showing results for 
Search instead for 
Did you mean: 

ADC

SRAM.11
Associate III

In my project I am using STM32G030k8, in which I need to use 6 ADC channels and 2 of them are Pa11 and PA12

PA9 and PA8 as gpio .

I couldn't able to configure PA11 and PA12 what is the alternate way to use that channel

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Peter BENSCH
ST Employee

RM0454 describes in section 14.3.8 that in mode Fully Configurable only inputs 0...14 can be used, which is also shown in STM32CubeMX. If you want to use ADC1.IN15 and higher, you have to set the ADC to Not Fully Configurable.

Does it answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Issamos
Lead III

Hello @SRAM.11 

If you want to make PA12 and PA11 as ADC_IN16 and ADC_IN15 you need to take a look at RM0454 ADC section. And the DS12991 to understand the mapping of ADC channels.

Best regards.

II

Yes ,Thank you so much.

Thank you.

 

Hi As per my old conversation I got my prototype to with the above adc channel I set the configuration as Not fully configurable and tried to build the project,I am getting same values for all the channels.I used conversion both by polling and DMA using interrupts I am getting the same results.How can I use the PA12 and PA11 channel in stm32G03ok8