STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST Bootloader behavior when flash is not programmed

Hi everyone!I found the following diagramm in AN2606 and my understanding was, that the bootloader will be executed when there is no valid content in flash memory.I know that boot pins or a jump from user code can be used to enter the ST bootloader, ...

kf_SEA_0-1711459809997.png
kf_SEA by Associate II
  • 1157 Views
  • 1 replies
  • 0 kudos

How to Include HAL Libraries into Already Existing Project

Hello,I am using an STM32F407G-DISC1 to run an open source program called Picovoice. More specifically their project at the following link (https://github.com/Picovoice/picovoice/tree/master/demo/mcu/stm32f407/stm32f407g-disc1). Unfortunately they do...

GSkoumal by Associate II
  • 8165 Views
  • 8 replies
  • 1 kudos

[Resolved] USART Tx pin sinks rx pin. HAL UART bug?

Edit: I found the problem, and it is of course my own fault. Careful reading of the transceiver chip datasheet reveals that the Rx pin follows the Tx pin by design on some models, including mine. Leaving this post up for posterity. I'm having an issu...

AntonL by Associate
  • 1402 Views
  • 0 replies
  • 0 kudos

Clarify stack management on STM32H7 / cortex M7

Hello,I'm a bit confused about stack management on Cortex M7.In my SW I only use the MSP.I understood that the MSP can only be modified with a MSR instruction. However the SP can be modified with a "simple" LDR instruction.Does that mean that when I ...

Gpeti by Senior II
  • 1422 Views
  • 1 replies
  • 0 kudos

Resolved! AN6091 ('L0->'U0 migration) comments

This is not a discussion on the 'U0 as such (that'd need some time to sink in); just comment on the 'L0->'U0 migration document, AN6091. It's a very detailed and extensive document, and following items are just relatively insignificant minor issues/t...

Bootloader to Main Appilication - SRAM Cleaning

hi,how to clean SRAM before jumping to main application from bootloader .In the SD card boot loader code we use local , global  & static variable and what will happen to these variables during the transition from boot loader to main application .how ...

MMARI.1 by Senior II
  • 891 Views
  • 0 replies
  • 0 kudos

Resolved! STM32H7B3I-DK - LCD init through .ioc file does not work

As I mentioned earlier I am trying to show red color on display screen this time using HAL_drivers. I attached a video on my one drive of me configuring a .ioc file and I builded it with 0 errors but when I flashed it to hardware, display module does...

richi by Associate III
  • 1755 Views
  • 2 replies
  • 0 kudos

Which code in SRAM4 for LPBAM?

Hello,In the example projects for LPBAM from ST, it is necessary to switch the RAM address to the SRAM region. This is because LPDMA has in Stop2-Mode only access to SRAM4.If I also want to use the RAM, which part of LPBAM (or maybe other parts) must...

JoachimO_0-1710411635664.png
JoachimO by Associate II
  • 1705 Views
  • 2 replies
  • 0 kudos