STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 has a FMAC, can it be tweaked to implement FFT?

STM32H7 has a FMAC (Filter mathematical accelerator), and FFT also build on multiply-accumulation operations similar to the filters. So, can the FMAC be tweaked to implement FFT with minimum MCU intervention. ​And also FFT calculation with M7 core wi...

YDao.1 by Associate
  • 3028 Views
  • 1 replies
  • 1 kudos

Resolved! CAN frame monitoring problem in loopback mode

@mƎALLEm hello again,   So , i am facing a problem to display the frame i am supposed to send from CAN_Tx pin in loopback mode. I am using picoscope to display. Here is the function i wrote to configure the Header, and send the data: void CAN_send(...

Erwan03 by Associate III
  • 4677 Views
  • 6 replies
  • 3 kudos

Resolved! Issue with CAN in loopback mode

Hello, i am using f446re nucleo board and have been facing a problem for a while now. I need to establish a loopback CAN transmission and the debug mode allows me to find a bug in the CAN Start function: HAL_ERROR 0x1 returned everytime i attempt. he...

Erwan03 by Associate III
  • 4080 Views
  • 7 replies
  • 2 kudos

Resolved! A bit disappointed about the STM32H7R/S lines

Dear ST,I was pleased to hear about the new STM32H7R/S lines, especially with the new graphic acceleration features in the R-line.However, and perhaps I have missed something, but I have to admit I am also disappointed about the absence of large size...

Resolved! 'H7 infographics: SMPS in 'H725?

DS says otherwise - that SMPS is available in *all* packages for 'H725: To me it appears that it's the infographics which is wrong. Wasn't the footnote supposed to go into some other sub-family?JW

waclawekjan_0-1708770806068.png waclawekjan_1-1708770917536.png

Resolved! Memory map of stm32f777zi

Hello,I am not able to find the memory map for the processors stm32f777zitx.It tells to refer to product line reference manual what does that mean?I checked everywhere on the internet but could not find it. 

rohan_m_0-1711364969324.png
rohan_m by Senior
  • 1826 Views
  • 2 replies
  • 2 kudos

Resolved! How to receive data from UART using STM32f746-Disco

Hi, I got a problem with the reception using USART7. I'm using it in the interrupt mode but the problem is that the data in the buffer is not coming well. I'm connecting STM32F407 board with the STM32F746 using UART. When the F7 transmits, there's no...

ferdlf by Associate III
  • 2407 Views
  • 4 replies
  • 1 kudos

What are the benefits of using LPBAM

Hi,I'm using STM32U575I-EV and CubeMX.Please tell me about benefits using lpbam in CubeMX.I thought that if I properly set up the peripherals that support LPBAM on the "Pinout & Configuration" screen, I could do the same thing as LPBAM Scenario.When ...

DK3 by Associate II
  • 1139 Views
  • 1 replies
  • 1 kudos