STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H723ZG reading vref problem

Hello, i am trying to read internal temperature and vref values from ADC3. I shared ADC3 ioc settings. ADC clock mux freq is 96MHz and sampling time is set to ADC3_SAMPLETIME_247CYCLES_5.On init routine calibration line as below :HAL_ADCEx_Calibratio...

iocADc.PNG
Enes1 by Associate
  • 982 Views
  • 0 replies
  • 0 kudos

Infrequently getting UNALIGNED HardFault

Hello There,I'm working on a FREERTOS based STM32H7A3 application.Upon debugging, my code randomly halts on UNALIGNED hardfault. The occurrence of this fault condition is very rare. During my testing in the last 30days, I ran into this for nearly 3 t...

KAgga1_0-1712212064993.png KAgga1_1-1712212107019.png KAgga1_2-1712212277969.png KAgga1_3-1712212424110.png
KAgga.1 by Associate III
  • 1877 Views
  • 2 replies
  • 0 kudos

Resolved! STM32 IC's Unique ID

Hi,I am using STM32G491RE MCU for my project. Is it true each STM32 IC has its own unique ID. For STM32G4 product has the UID facility. Is it 96-bit ID for all the stm32 families or is it different.Which manual has to be referred for this?If yes can ...

[STM32h7] ADC3 BDMA Transfer error (Buffer located in SRAM4)

I understand the STM32H7's BDMA requires special attention to the memory map [FAQ: DMA is not working on STM32H7 devices]however, when I try to declare the buffer to SRAM4 that will be the destination for the ADC DMA transfer, __attribute__((at(0x380...

EZamo.1 by Associate III
  • 6041 Views
  • 6 replies
  • 0 kudos

Resolved! USB FS Support

I am working on OTG FS application on stm32f769 discovery board, as per the it's schematic for OTG_FS VBUS power supply will be taken care by External Phy(see below image). So as per that I configure the STMCUBE IDE, and i disabled the VBUS_Sensing a...

Shikamaru_0-1711460081875.png
Shikamaru by Associate III
  • 2734 Views
  • 4 replies
  • 1 kudos

STM32H563ZI LINKER

Hi,I am working on freertos plus tcp library with STM32H563ZI, but how must I make memory otions in linker file?like: RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 320KFLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048KRAM1 (xrw) : ORIGIN = 0x20000000, LENG...

Recep by Associate II
  • 8446 Views
  • 11 replies
  • 2 kudos

How to write Product serial number in STM32H7

I am making a product and trying to write a serial number. After looking into it, I heard that I can use the unique device ID to write the serial number, but I understand that the unique device ID is read-only. I am curious as to whether the previous...

jink by Associate
  • 1764 Views
  • 2 replies
  • 0 kudos

Resolved! USB clock source about STM32U595 can use HSI?

The datasheet say:USB on-the-go high-speed (OTG_HS)     The devices embed an USB OTG high-speed device/host/OTG peripheral with integrated transceivers. The OTG_HS peripheral is compliant with the USB 2.0 specification and with the OTG 2.0 specificat...

Barfield by Associate II
  • 2011 Views
  • 2 replies
  • 1 kudos

STM32L476RG UART with DMA using Reception Till Idle

I've encountered an issue while implementing code on an STM32L476RG Nucleo board to receive variable-length data from Tera Term using USART2 in asynchronous mode. The baud rate is set to 1 Mbps with a 16 MHz sysclk. However, the code doesn't accurate...

Devesh by Associate
  • 2411 Views
  • 2 replies
  • 0 kudos