Skip to main content
Associate
December 14, 2023
Question

STM32 RS485通讯 - 在2.5Mbps波特率下可以接收数据吗?

  • December 14, 2023
  • 1 reply
  • 903 views

STM32F051C8T6产品,想用来和多摩川的编码器产品通讯,发送数据0x02,多摩川编码器发送6个字节返回。但用6个字节的中断得不到数据,用6个字节读取也无法得到数据。中断只能收到一个字节,02。有指导问题出在哪里了?

    This topic has been closed for replies.

    1 reply

    Lina_DABASINSKAITE
    ST Community Manager
    December 14, 2023

    TRANSLATION: 
    STM32 RS485 Communication - Can I receive data at 2.5Mbps baud rate?

    STM32F051C8T6 product, I want to use it to communicate with Tamagawa's encoder product, send data 0x02, Tamagawa encoder sends 6 bytes back. But I can't get data with 6 bytes interrupt, and I can't get data with 6 bytes read. The interrupt can only receive a byte, 02. there is a guide to where the problem is?

    ​In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.