STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401RCT6 requires a reset to run code

We have a new revision that has a significant population of boards with this intermittent power issue. steps to reproducepress power buttonpower applied to the MCU the MCU only prints a single debug message, then haltspress reset: device works normal...

OCTOSPI line idle level - Weird behaviour

Hi, Community,I'm trying to understand the OCTOSPI peripheral on my STM32L4P5. I'm new to STM32, but old in embedded. Particularly, I need to know/affect the idle level of the data line of the OCTOSPI. I thought that the last transmitted bit would re...

DS0002.png DS0001.png

STM32 Phase Vocoder Algorithm

Hi! I'm looking to implement a phase vocoder algorithm on an STM32F4/STM32F7 and I was wondering if anyone has already done this and can provide suitable resources?Thanks!

Resolved! UART TX and RX pin issue

Hello,I am using "NUCLEO-H743Zi2" eval board. I am using it for UART communication. I had configured UART4 in it as following;PA0 as UART4_TXPA1 as UART4_RXWhen I tried to transmit, it is not transmitting more than 2 bytes. While receiving, it is not...

adithya_sharma_0-1712761586212.png

I2C Slave Receive in DMA mode on STM32U575 series

Hi,I'm attempting to set up an STM32U575 as an I2C slave. (The master is a F301)My problem is that the slave only receives one byte, and then proceeds to disregard all of the following data.I have set up a switch that turns on an RGB LED, depending o...

Screenshot 2024-04-11 at 05.51.14.png Screenshot 2024-04-11 at 05.53.02.png Screenshot 2024-04-11 at 06.00.40.png Screenshot 2024-04-11 at 06.15.33.png

Resolved! stm32l431rct HardFault using spi, adc , RTOS

Hello im Khoi. i get big trouble with stm32l431rct, when i using freeRtos . Task1 i using spi comunication . Task2 i get ADC DMA . When i disable Task2 program no problem. But i enable task2 get problem spi hardfault-Handler . Excuse me :(( 

Resolved! bluetooth communication problem when working with two UARTs

Hi during development of program I found weird behaviour. I am using STM32G030C8T6 MCU. I am trying to connect external device using HC-05 bluetooth module. In my project I also connect with devices using MAX3485 module for RS485 communication. I wro...

MaciejG by Associate II
  • 2039 Views
  • 3 replies
  • 2 kudos

Ux_Device_HID for STM32U575ZI

Hello,I wonder if it exists an Ux_Device_HID example project for STM32U585ZITxQ mcu or the way to convert the Ux_Device_HID project for STM32U585AIIXQ present in the examples for a different packaged mcu. Best regardsIlaria

Ilaria by Associate
  • 1549 Views
  • 3 replies
  • 0 kudos