In the case where USB power is first applied and a 20V contract established, the STUSB4500 would enable the power path to Vsnk as per usual. Then assume a 20.9V (for example) secondary power source is applied to the Vsnk output (say from a wall adapt...
Also, will the VBUS_EN_SNK pin get asserted (pulled low) in this case, allowing the power path to enable 5V from the USB 2.0 cable to power the device?
Posted on April 27, 2018 at 23:51 STM32F407VETxBlank CubeMX project template plus USB_DEVICE middleware using CDC classSW4STM32firmware STM32Cube FW_F4 V1.16.0only modified code from generated templates is this (in main.c): /* USER CODE BEGIN 2 */...
Posted on August 01, 2016 at 16:02
Overall objective: Using
https://github.com/groupgets/purethermal1-firmware as a base, add a USB serial port interface (which would replace the DEBUG functionality it has currently).
I have read thro...
Posted on March 31, 2016 at 15:28I'd like to know if the STL62P3LLH6 P-channel MOSFET's Safe Operating Area chart is correct in http://www.st.com/web/en/resource/technical/document/datasheet/DM00105886.pdfhttp://www.st.com/web/en/resource/technical/...
Posted on June 11, 2017 at 02:06 The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=06...
Posted on August 15, 2016 at 01:01
Are these endpoint values OK:
UVC_IN_EP 0x81
UVC_CMD_EP 0x82
CDC_IN_EP 0x83
CDC_OUT_EP 0x03
CDC_CMD_EP 0x84
I used Wireshark's USB capture and compared it to debug output from the micro's USART out...
Posted on March 31, 2016 at 15:27The online support has never worked for me. I always get a ''Serena Single Sign On Invalid User ID or Password.''error when I try to access it which is why I post questions on the forum instead. Thank you for your su...