STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F205RGTx to E220-400T22D LoRa Communication Issue

Hello everyone,I'm currently working on a project involving the STM32F205RGTx MCU and the E220-400T22D LoRa module. I'm trying to send the command "C0 04 01 09" from my STM32 to the LoRa module, but it seems that the command isn't being recognized co...

Resolved! How to Configure multiple FD CAN RX_BUFFER ?

Hello,I configured my FD CAN on NUCLEO STM32H53 with the function as below. I want to have two RX Buffers to receive 2 specific CAN IDs. However, when I checked RX_BUFFER0 with if (HAL_FDCAN_IsRxBufferMessageAvailable(&hfdcan1, FDCAN_RX_BUFFER0) > 0...

ANguy.5 by Associate II
  • 4074 Views
  • 3 replies
  • 1 kudos

First test with "Blinking Led", but error message

Hello to everyoneI have connected a NUCLEO F446RE board, and I was following the tutorial "Step 2, Blinking LED" In the end, after launching the Debug, I receive the following error message.What does it mean? How can I solve?Tanks to anyone who will ...

FabioCC by Associate II
  • 2440 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer USB connect stalls at “IAP”

Hi there, folks. I hope someone familiar with this product can help me. I am trying to update the firmware in a Malahit DSP2 radio receiver that is powered by an STM32H743 MCU. I am following the manufacturer’s procedure, which utilizes STM32CubeProg...

JMora by Associate II
  • 2112 Views
  • 1 replies
  • 1 kudos

Resolved! F469i-Disco CAN receive issues

Hello dear ST community,   we want to use the STM32F469i as a Dashboard in our Formula Student car but we are having trouble receiving any can data whilst transmitting works just fine. We tried allot allready but nothing has worked for us so far.We a...

Bild (5).png

Resolved! STM32F105 using only CAN2 module

I'm using a STM32F105 MCU on which I want to use only the CAN 2 Module to communicate. The pins for the CAN1 Module are used for other stuff. Currently I'm setting the init parameters for CAN1 and CAN2 but CAN1 is never startet. On the low level init...

taca_vi by Associate
  • 2011 Views
  • 2 replies
  • 1 kudos

stm32h732 matrix-vector multiply throughput

I am trying to gain an appreciation of how much f32 128x128 element matrix-vector multiply compute I should expect from this type of processor (for the purpose of running small control neural networks on the m7 core).As I understand the m7 core, it s...

Eelco by Associate II
  • 7771 Views
  • 17 replies
  • 1 kudos