STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 SPI receive always shifted 3-4 bytes

Posted on January 15, 2017 at 18:50Hallo,  i use the HAL to program a little test software to transfer data via spi between two STM32 Nucleo boards.One board with a STM32L476 sends every 5 ms 74 bytes of data as a spi master with 625 kBit.Chip selec...

volker2 by Associate II
  • 11766 Views
  • 19 replies
  • 0 kudos

STM32F103: Sometimes USART stops working

Hi, We are using STM32F103 in our project. Established IPC communication over USART. We have almost finished our development. We kept our setup running for long, sometimes we found that IPC-USART communication getting stuck, IPC does not work until w...

[STM32F373RC] Question about using flash memory like EEPROM.

Hi.I want to save and load data to flash memory. (STM32F373RC)And initialization code was generated through cubemx.All functions including SPI, I2C, and ADC were successfully tested.However, saving and loading data into flash memory failed.All functi...

YS4 by Associate
  • 1502 Views
  • 2 replies
  • 0 kudos

Resolved! Nucleo U575ZI-Q DCMI

Hello forum, I'm starting to develop a smart robotic system, I wanted to base the movement part on an STM32 micro-controller,We thought about basing our SLAM on a camera and a simple distance sensor (and an IMU of course) for the initial mapping. the...

Timer Compare Output using DMA - STM32F3Discovery

Hello,I am attempting to generate a waveform with a period of 33ms. In-between each period, I need to toggle the timer output 5 times with a varying timescale. My initial thought is to do this using a timer in output compare mode and then update the ...

daded1_1-1715401969734.png daded1_3-1715402159278.png daded1_4-1715402178719.png daded1_5-1715402229843.png
daded.1 by Associate II
  • 4731 Views
  • 4 replies
  • 1 kudos

Resolved! Simple Ranging Error

Hi I'm new to the STM32 series, I have a NUCLEO-F401RE and the X-NUCLEO-53L8A1. I am trying to edit the code from the X-CUBE-TOF1 SW package but run into the error below when compiling. Any ideas on how to resolve this issue?  Log output file: C:\Use...

Buntice by Associate II
  • 4959 Views
  • 3 replies
  • 3 kudos

Manual Keyboard Detection

hi,USB keyboard working fine via HID and i need have small Manual Keyboard Detection  by pressing button . it's not compiling  if( HAL_GPIO_ReadPin(GPIOC, button_Pin)) { if(USBH_HID_GetDeviceType(USBH_HandleTypeDef *phost) == HID_KEYBOARD)...

MMARI.1 by Senior II
  • 2054 Views
  • 3 replies
  • 1 kudos

Resolved! BOOT_ADD0 and BOOT_ADD1 are programmed with values 0xFFFF

Hi,I am using an STM32F746IE controller and in some of them i don't see proper ST programmed values in address locations of BOOT_ADD0 (0x1FFF 0010) and BOOT_ADD1 (0x1FFF 0018). As per the reference manual i understand the ST programmed values in thes...

3b004d21-7006-4235-8414-87c52f055602.jpg