cancel
Showing results for 
Search instead for 
Did you mean: 

USB gadget

Barak1
Associate

 

I have successfully configured USB On-The-Go (OTG) on an STM32 microcontroller to support both Abstract Control Model (ACM) and Human Interface Device (HID) protocols. I utilized the stm32_usbotg_eth_config.sh script as a reference, and the setup is functioning as intended.

Now, I am seeking guidance on modifying the USB configuration to initially support only the HID protocol. Subsequently, I aim to dynamically enable the ACM protocol when specific events occur. To achieve this, I have adapted the script to exclusively open the HID protocol and created another script to open the ACM protocol as well.

While the second script is functional, I have observed that in order to detect the ACM functionality on my Windows computer, I need to disable the gadget (echo "" > UDC) and then re-enable it (echo $(ls -1 /sys/class/udc/ > UDC)) as per the kernel reference.

Is there a method to append an additional function without the need to disable and enable the UDC, or alternatively, is there a way to activate or deactivate functions dynamically while the USB gadget is still operational?

Your insights and guidance on this matter would be greatly appreciated.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Douglas MILLER
ST Employee

This forum thread was marked by the moderator as needing a little more investigation, so a Support case was created in your name and will be handled off-line.