STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Dynamic phase shift

Hi,My goal is to dynamically change the phase shift between two output signals. Ultimately I would like to do this by rotating an encoder knob, but for the sake of simplicity a software change will do to simplify things. I'm using a Blue pill (STM32F...

llaabbss by Associate II
  • 6739 Views
  • 5 replies
  • 2 kudos

Resolved! Stm32h743I using ethernet in Lwip middleware

Hii I'm currently working stm32h743IITx 176  pins stm32cube mx v 6.2.0 . i used ethernet in lwip middleware are used my currently using firmware version 1.9.1 but couldn't connect udp cilent in ethernet   .  No ping, no nothing. Currently I test with...

Resolved! Register bits missing in STM32CubeProgrammer

I stumbled across this problem:https://community.st.com/t5/stm32-mcus-products/unable-to-read-reset-values-of-the-stm32h730vb-octospim/m-p/212094In the current rev 3 of RM0468 https://www.st.com/resource/en/reference_manual/rm0468-stm32h723733-stm32h...

pkoevesdi_2-1715444936114.png pkoevesdi_1-1715444512232.png

Resolved! Command sequence for USART bootloader on stm32G4 MCU

Hello, I am trying to flash the MCU with USART bootloaderI am using the command codes from below link, but are not working for meCan someone help me validate of the command codes are correct for STM32G4https://www.st.com/resource/en/application_note/...

Resolved! STM32G0B1V FDCAN AutoRetransmission

Hallo everybody, I have a question about the FDCAN peripheral of the STM32G0B1VC.I’m using the STM32Cube_FW_G0_V1.6.0 library and I have initialized the bus with AutoRetransmission:CanHandle.Init.AutoRetransmission     = ENABLE; During the transmissi...

g0_ScreenDump.png f0_ScreenDump.png
Thomas1 by Associate II
  • 3901 Views
  • 4 replies
  • 1 kudos

OTG on STM32F7 controller

Hi team,             Is there any sample of OTG MSC on F7 controller. Need both Host and Device stack on single application. Based on the ID pin need to decide which one to run.  For Host - If i connect an USB stick to controller, it can read and wri...

Shikamaru by Associate III
  • 1357 Views
  • 2 replies
  • 1 kudos

Resolved! unstable custom delay function (STM32 & STM32CubeIde)

 Hello,I have a small problem when using a custom delay function as follows : void delay_us(uint32_t delayus) { uint32_t start_count = __HAL_TIM_GET_COUNTER(&htim2); while ((__HAL_TIM_GET_COUNTER(&htim2) - start_count) < delayus) { } }  The attac...

LadyMt by Associate III
  • 9153 Views
  • 18 replies
  • 3 kudos

How to take ADC data at 166ksps with calculation

I want to take ADC data at 166ksps but I am getting after 2 second. Can anyone suggest How can I take ADC data and also perform calculation ? Please give some guidance. I am attaching my main.c file.

ms10 by Associate
  • 2717 Views
  • 3 replies
  • 0 kudos