STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Clock cycle shift on GPIO output STM32F103

Dear Community,I am porting an old application made on AVR to STM32, and I am facing a strange timing issue. In a nutshell, the application is reading sector (512 Bytes) from a SDCARD and output the content of the buffer to GPIO with 4us cycle (meani...

Screenshot 2024-05-12 at 06.30.59.png Screenshot 2024-05-12 at 06.32.34.png
vbesson by Senior
  • 25420 Views
  • 40 replies
  • 3 kudos

STM32 Timer 8 ETR pin behaving as output

Hello Team,I am using an STM32F469NIH6 in my project and the following is my use case: I need the timer 8 to act as a slave to its ETR pin, which is PA0. I have a signal coming out on the PG7 from my daughter board and I have connected PG7 and PA0 vi...

Jansunil_1-1716800431150.png Jansunil_2-1716800447179.png
Jansunil by Associate II
  • 2619 Views
  • 4 replies
  • 0 kudos

Resolved! SMBus on STM32C031

Hi ST tesam,When I use  HAL_SMBUS_Master_Receive_IT( ) to receive data from device ,I can not got the information directly after the HAL_SMBUS_MasterRxCpltCallback( SMBUS_HandleTypeDef *hsmbus ) was complete.(I had set a flag when HAL_SMBUS_MasterRxC...

LsnLeeJW by Associate II
  • 3280 Views
  • 4 replies
  • 0 kudos

Resolved! STM32 downstream of a USB hub

Hi !An application I am working on has a PC connecting to an ethernet device (currently through Ethernet) and a STM32 (STM32G0B0CET6) through USB.I am looking to only have one connection to the PC through USB, hence I am looking to have the incoming ...

4lch by Associate II
  • 2608 Views
  • 4 replies
  • 2 kudos

error from compiler (linker) - NUCLEO-F072

Hi I m using F072 Nucleo bd, and compiler report the following errors but there was no syntax error from the code, can anyone advise?22:08:09 **** Incremental Build of configuration Debug for project F072_GPS_ NEO-6M_i2c_LCD_16x2 ****make -j8 allarm-...

Resolved! Error with STM32CubeMx 6.11.1

Hi,I'm working on a STM32H755BIT6 with a custom PCB layout, which uses direct SMPS supply hardware configuration.I'm migrating an existing Keil project which was created with STM32CubeMx 6.7.0 to STM32CubeMx 6.11.1 and I discovered that the option PW...

RTira1_0-1716816356297.png RTira1_1-1716816492159.png RTira1_2-1716816598403.png
RTira.1 by Associate II
  • 1827 Views
  • 3 replies
  • 0 kudos

STM32L051K8 writing half page to EEPROM?

I'm using an STM32L051K8. I'm writing words to EEPROM. It takes a lot of time to do that. I read in the datasheet that it is possible to do a half-page write that will take the same amount of time as a single write. How do I write a half page? Do I u...

MSipo_0-1716821817404.png MSipo_1-1716821849160.png MSipo_2-1716821868344.png
MSipo by Senior II
  • 846 Views
  • 0 replies
  • 0 kudos